2.37.6 ECIA_GIRQIsInterruptEnabled Function
C
bool ECIA_GIRQIsInterruptEnabled(ECIA_INT_SOURCE int_src)
Summary
Returns the status of the given interrupt source
Description
Returns true if the interrupt source is enabled ; returns false otherwise.
Precondition
None.
Parameters
Param | Description |
---|---|
int_src | One of the interrupt source from the enum ECIA_INT_SOURCE |
Returns
true - interrupt source is enabled false - interrupt source is disabled
Example
bool status = ECIA_GIRQIsInterruptEnabled(ECIA_AGG_INT_SRC_GPIO002);
Remarks
None