2.110.17 SUPC_BOD33_CALLBACK Typedef

C

typedef void (*SUPC_BOD33_CALLBACK)( uintptr_t context );

Summary

Defines the data type and function signature for the SUPC peripheral callback function.

Description

This data type defines the function signature for the SUPC peripheral callback function. The SUPC peripheral library will call back the client's function with this signature when a Brown Out event has been detected. The function will be called only if the BOD33 action in the NVM user row is set to interrupt.

Remarks

SUPC_Initialize() must have been called for the supc peripheral before registering a callback. SUPC_BOD33CallbackRegister() must have been called to set the function to be called.

Parameters

ParamDescription
contextAllows the caller to provide a context value (usually a pointer to the callers context for multi-instance clients).

Returns

None.

Example

void APP_BrownOutEventHandler( uintptr_t context )
{
    // Code to perform any quick action before the supply dies.
}

SUPC_BOD33CallbackRegister(APP_BrownOutEventHandler, 0);

Remarks

None.