2.131.39 USARTx_LIN_NodeActionSet Function
C
/* x = USART instance number */
/* Blocking and Ring buffer mode */
void USARTx_LIN_NodeActionSet( USART_LIN_NACT action )
Summary
This API allows the application to set LIN Node Action (PUBLISH, SUBSCRIBE or IGNORE)
Description
This API allows the application to set the Action to be performed by LIN Node (PUBLISH, SUBSCRIBE or IGNORE)
Precondition
USARTx_Initialize must have been called for the associated USART instance.
Parameters
| Param | Description |
|---|---|
| action | Action to be performed by the node which is defined by enum type USART_LIN_NACT |
Returns
None
Example
USART0_LIN_NodeActionSet( USART_LIN_NACT_PUBLISH )
Remarks
None