2.131.38 USARTx_LIN_IdentifierWrite Function
C
/* x = USART instance number */
/* Blocking and Ring buffer mode */
bool USARTx_LIN_IdentifierWrite( uint8_t id)
Summary
This API allows the application to set LIN Node ID which is part of LIN Header
Description
This API allows the application to set LIN Node ID which is part of LIN Header
Precondition
USARTx_Initialize must have been called for the associated USART instance.
Parameters
| Param | Description |
|---|---|
| id | LIN ID to be set during transmission of LIN header |
Returns
API returns True or False indicating success or fail to set the LIN Id
Example
uint8_t txBuffer[10]; void LIN_MasterTransmit(uint8_t pid, uint8_t* pData, uint8_t nBytes) { nTxBytes = 0; while (nBytes--) { txBuffer[nTxBytes++] = *pData++; } USART0_LIN_ResponseDataLenSet(LIN_NUM_OF_BYTES_TRANSFER_FROM_HOST_TO_CLIENT); /* Transmit- PID */ USART0_LIN_IdentifierWrite(pid); /* Transmit- DATA + CHECKSUM */ USART0_Write(txBuffer, nTxBytes); }
Remarks
None