2.73.31 NVMCTRL_DisableSmartEepromInterruptSource Function
C
void NVMCTRL_DisableSmartEepromInterruptSource(NVMCTRL_INTERRUPT1_SOURCE int_source)
Summary
Disables a given interrupt source for the SmartEEPROM.
Description
There are multiple interrupt sources supported by the NVMCTRL peripheral. It supports two interrupt vectors, one for interrupts from the SmartEEPROM and another for all other interrupts of the NVMCTRL. This function disables the given interrupt for the second vector which is used by all interrupts from the SmartEEPROM.
Precondition
Interrupt option in MCC should have been enabled.
Parameters
Param | Description |
---|---|
int_source | Refer to enum NVMCTRL_INTERRUPT1_SOURCE for possible values. |
Returns
None.
Example
NVMCTRL_DisableSmartEepromInterruptSource(NVMCTRL_INT_SEEWRC);
Remarks
This API is available only if the SmartEEPROM interrupt is enabled via the MCC tree.