3.2.26.1 DIAG_TC_Disable
Returns the status of the TC_DISABLE diagnostic
This function disables the peripheral, then verifies that it has been
disabled.
DIAG_TEST_STATUS
DIAG_TC_Disable
(
DIAG_TC_PERIPHS tc_periph
);Diagnostic verifies the following faults do not exist
- TC will not turn off
Operating Mode
- Interface can be used at POST and ‘On Demand’
Precondition
- none
Parameters
- tc_periph - enum value for which TC peripheral to be tested
Returns
- DIAG_TEST_PASSED if no faults were found, otherwise, DIAG_TEST_FAILED.