3.2.8.4 DIAG_DMAC_LinkedList
Returns the status of the DMA_LINKED_TRANSFER diagnostic
This function configures the DMAC to transfer a block of data from one SRAM location to another. Check that the request is carried out, with correct values for the source address, destination address, and data length.
DIAG_TEST_STATUS
DIAG_DMAC_LinkedList
(
int chan
);
Diagnostic verifies the following faults do not exist
- Error in linked list operation
Operating Mode
- Interface can be used at POST and ‘On Demand’
Precondition
- none
Parameters
- chan - DMAC channel (if negative, routine will choose one)
Returns
- DIAG_TEST_PASSED if no faults were found, otherwise, DIAG_TEST_FAILED.