9.18.3 FlashPro® Lite

For FlashPro® Lite, the existing 26-pin connector is shown in the figure below.

Figure 9-142. 26-pin Connector for FlashPro® Lite
???
Note: All ground pins must be connected. The rectangular shape shows connections on the programmer itself. Arrows show current flow towards or from the rectangular programmer.

The appropriate SAMTEC micro connector target cable for this is: Samtec FFSD-13-D-12.00-01-N.

The 12 inch cable is specified. This is likely to be more than enough to connect to the board and reducing the inductance will help compared with 18 inches, which is supplied by the default with FlashPro Lite.

See the following table for a description of the signals.

Table 9-40. FlashPro Lite Signal Description

Signal

Description

VDDP

VDD supply for logic I/O pads

VDDL

VDD supply for core

VPP

Positive programming supply (+16.5V)

VPN

Negative programming supply(-13.8V)

GND

Signal reference

SENSE

Input from target board to programmer to indicate connection to ground

TCK

JTAG clock

TDI

JTAG data input to device

TDO

JTAG data output from device

TMS

JTAG mode select

nTRST

Programmable output pin may be set to off, toggle, low, or high level

RCK/OUT0

Programmable output pin may be set to off, toggle, low, or high level

N/C

Programmer does not connect to this pin

Some designers of high-integrity boards (military and avionic) may arrange their boards so that TRST is tied to ground via a weak pull-down resistor. The purpose of this is to hold the JTAG state-machine in a reset state by default, so that even with TCK oscillating, some sudden ion bombardment or other electrical even will not suddenly throw the JTAG state-machine into an unknown state. If your design also uses a weak pull-down resistor on TRST on your board, then enabling the "Drive TRST" flag will be required to force the JTAG state-machine out of reset to permit programming to take place. With most boards, there is no need to select this flag.