15.4.5 Unassigning Pins
To unassign a macro from a pin:
- In the Hierarchy window (Logical or Physical tab), select the macro to unassign.
- From the Logic menu, choose Unassign From Location. This command is available only if the macro has been assigned to a location.
To unassign a macro from a region:
- In the Hierarchy window (Logical or Physical tab), select the macro to unassign.
- From the Logic menu, choose Unassign From Region. This command is available only if the macro has been assigned to a region.
Note: You can also right-click the macro, and choose Unassign From Region
or Unassign From Location.
To unassign all I/Os from a location, choose Unassign All From Location from the Logic menu. To unassign all I/Os from the selected region, choose Unassign All From Region from the Logic menu.