15.4.8 Setting PinEditor Properties
You can bring the selected macro into view in PinEditor by setting the Move the display to show Selected Macro or Module property.
This property brings the selected macro or module into view in the PinEditor window. By default, this property is selected. If you don't want to change your viewing area each time you select a macro or module, clear this check box.
To set PinEditor properties:
- From the View menu, choose Properties.
- In the PinEditor Properties dialog box, select the check box if you want to bring a macro or module into view when you select it, or clear the check box if you do not.
- Click OK.