14.15.3 Verilog Source File
Like the Constants in VHDL, Verilog library has two definitions:
`define AX_FF_INIT_VALUE 1'b0
`define POWERUP_TIME 100
AX_FF_INIT_VALUE defines the required power up state. POWERUP_TIME defines for how long GCLR and GPSET should be applied. You can modify these definitions as required and compile the library. Settings for power up states 0/1 are listed as follws.
POWER UP STATE = 1
Set the definition as:
`define AX_FF_INIT_VALUE 1
POWER UP STATE = 0
Set the definition as:
`define AX_FF_INIT_VALUE 0