14.15.2 VHDL Source file
Two constants are defined inside the VTABLES package:
constant AX_FF_INIT_VALUE : std_ulogic := '0'; constant POWERUP_TIME : time := 100 ns;
AX_FF_INIT_VALUE defines the required power up state; POWERUP_TIME defines for how long-GCLR and GPSET should be applied. You can modify these constants as required and compile the library. Settings for power up states 0/1 are listed as follows.
POWER UP STATE = 1
Set the following constant value in VTABLES package
constant AX_FF_INIT_VALUE : std_ulogic := '1';
POWER UP STATE = 0
Set the following value as in VTABLES package
constant AX_FF_INIT_VALUE : std_ulogic := '0';