9.13.5 Programming the FPGA Array
The FPGA Array contains user design. In FlashPro® for SmartFusion® devices, an FDB file is required to program the FPGA Array.
To program the FPGA Array:
- Select the FPGA Array silicon feature on the Generate Programming File page.
- Click OK to include the FPGA Array in the programming file.
When using a PDB that includes an FPGA Array, the FPGA Array cannot be deselected for programming, except when programming SmartFusion devices.
For more information, see the Generate a Programming File section.