9.13.17 Parallel Port Cable Information
The FlashPro® software supports the generic Parallel Port Cable.
To connect to the Parallel Port Cable:
- From the Parallel Port Cable text box, select the Parallel Port Buffer Cable.
- Select the parallel port that is connected to the
cable from the Parallel Port text box.
Figure 9-136. Connect Parallel Port Cable
- Click OK.
The Para2Buff programmer is added to the programmer list.