1.3.7.1 RTC Signals

All signals are active high.

NameTypeDirection
RTCCLKINPUTRTC Clock; must be driven by the XTLOUT of the XTLOSC macro
RTCXTLSELOUTPUTCrystal Oscillator select; must be connected to the XTLSEL on the XTLOSC macro
RTCXTLMODE[1:0]OUTPUTCrystal Oscillator mode select; must be connected to RTCXTLMODE on the XTLOSC macro
RTCMATCHOUTPUTMatch signal when match value reached
RTCPSMMATCHOUTPUTMatch signal when match value reached; must be connected to RTCMATCH of VRPSM macro. Exposed only if "Export Match signal for Voltage Regulator Power Supply Monitor" is enabled.

The following timing diagram displays accessing the ACM for the RTC values. In the diagram, the RTC counter is disabled. Then, the RTC match register is read and finally the match register is overwritten with a new value. The RTC is then re-enabled.

Figure 1-25. ASB RTC Access
???