5.24.20 Integrating Precision RTL
Libero IDE supports Precision RTL from Mentor Graphics.
To integrate Precision RTL with your Libero IDE project:
- From the Options menu, choose Profile. The Project Profile dialog box appears.
- Click Add and select Synthesis. The Add Tool dialog box appears.
- Enter a name. This is the name that appears in the Project Profile dialog box.
- Select Precision RTL.
- Enter the location of Precision RTL and any additional parameters.
- Click OK.
- Select Precision RTL in the Project Profile dialog box and click OK.
- Click Precision RTL in the Project Manager Project Flow window to start Precision RTL.