14.1.2 How to Use this Guide
Family Inclusion Indicator
In the titlebar of each macro is a list indicating whether the cell is a member of the ACT 1, ACT 2, 3200DX, ACT 3, MX, SX, SX-A, eX, or Axcelerator library.
Guidelines
- All input pin loading is assumed to be a single load except macros that are built using two combinational modules or one sequential and one combinatorial module. These macros are assumed to have a load of two on some of their input pins.
- All macros have output pin loading of zero except for the sequential macros that are built using two combinational modules only. These macros have an output pin loading of one.
- All macros have logic levels equal to one except cells with pin delays of two. A “2” is added to the corresponding symbol in the macro section of this manual.
Truth Table Nomenclature
Truth tables are arranged with Inputs before Outputs. The following symbol definitions apply
↑ denotes rising edge clock
↓ denotes falling edge clock
X in an input column denotes a ‘don't care’ or logic simulation state ‘unknown
!Q denotes Q not
Pin Delay Annotation
Two-module combinatorial macros contain extra delay on some or all of the pins. If a macro symbol in this guide displays a “2” on a pin, then two levels of logic delay exist on the input to output path.
Note: Many two-level logic functions in one family are implemented
in a single module in another family, hence the “2” may apply to specific families
only.