21.8.44 remove_multicycle_path

Description

Removes a multicycle path constraint from the current timing scenario by specifying either its exact arguments or its ID. If the arguments do not match a multicycle path constraint in the current scenario, or if the specified ID does not refer to a multicycle path constraint, this command fails.
Note: Do not specify both multicycle path arguments and the constraint ID.
remove_multicycle_path [-from from_list] [-to to_list] [-through through_list]
remove_multicycle_path -id constraint_ID

Arguments

ParameterTypeDescription
fromlist of stringsSpecifies a list of timing path starting points. A valid timing starting point is a clock, a primary input, an inout port, or a clock pin of a sequential cell.
throughlist of stringsSpecifies a list of pins, ports, cells, or nets through which the disabled paths must pass.
tolist of stringsSpecifies a list of timing path ending points. A valid timing ending point is a clock, a primary output, an inout port, or a data pin of a sequential cell.
idstringSpecifies the ID of the multicycle path constraint to remove from the current scenario. Specify either the exact multicycle path arguments to remove or the constraint ID that refers to the multicycle path constraint to remove.

Error Codes

Error CodeDescription
NoneOnly one argument is needed.

Supported Families

PolarFire®
PolarFire SoC
SmartFusion® 2
IGLOO® 2
RTG4

Exceptions

You cannot use wildcards when specifying a clock name, either alone or in an accessor command such as get_pins or get_ports.

Example

The following example specifies all the multicycle paths between reg1 and reg2.

remove_multicycle_path -from [get_pins {reg1}] -to [get_pins {reg2}]

Related Examples on GitHub

See Also