21.8.54 set_clock_uncertainty
(Ask a Question)Description
Specifies simple clock uncertainty for single clock and clock-to-clock uncertainty between two clocks (from and to).
The set_clock_uncertainty
command sets the timing uncertainty of
clock networks. It can be used to model clock jitter or add guard band in timing
analysis.
SmartTime computes uncertainty values very similar to the
set_clock_latency
command (when used with the
-early
and -late
arguments), but with one
difference in the timing report. Uncertainty number is always applied to the
required time calculation whereas latency numbers are applied to both arrival and
required time. Uncertainty is added for both setup and hold checks.
set_clock_uncertainty
command, you must explicitly use
-setup
argument. If the -setup
argument is not
specified, SmartTime will apply the uncertainty value to both setup and hold
calculations leading to incorrect jitter modeling.-setup used |
-hold used |
Result |
---|---|---|
No | No | Setup and hold checks. |
No | Yes | Hold checks only. |
Yes | No | Setup checks only. For jitter modeling. |
Yes | Yes | Setup and hold checks. |
Either simple clock uncertainty or clock-to-clock uncertainty can be specified.
Simple clock uncertainty can be set on a clock or on any pin in the clock network.
It will then apply to any path with the capturing register in the forward cone of
the uncertainty. If multiple simple uncertainty applies to a register, the last one
(in the propagation order from the clock source to the register) is used.
Clock-to-clock uncertainty applies to inter-clock paths. Both from
clock and to
clock must be specified. Clock-to-clock uncertainty
has higher priority than simple uncertainty. If both are set (a clock-to-clock
uncertainty and a simple clock uncertainty on the to
clock), the
simple clock uncertainty will be ignored for inter-clock paths, only the
clock-to-clock uncertainty will be used.
set_clock_uncertainty [-setup] [-hold] uncertainty [object_list -from from_clock |
-rise_from rise_from_clock | -fall_from fall_from_clock -to to_clock | -rise_to rise_to_clock |
-fall_to fall_to_clock ]
Arguments
Parameter | Type | Description |
---|---|---|
uncertainty | floating point | Specifies the time in nanoseconds that represents the amount of variation between two clock edges. |
object_list | list of strings | Specifies a list of clocks, ports, or pins for simple uncertainty; the uncertainty is applied either to destination flops clocked by one of the clocks in the object list option, or destination flops whose clock pins are in the fanout of a port or a pin specified in the object_list option. |
from | list of strings | Specifies that the clock-to-clock uncertainty applies to both rising and falling edges of the source clock list. Only one of the -from , -rise_from , or -fall_from arguments can be specified for the constraint to be valid. |
rise_from | list of strings | Specifies that the clock-to-clock uncertainty applies only to rising edges of the source clock list. Only one of the -from , -rise_from , or -fall_from arguments can be specified for the constraint to be valid. |
fall_from | list of strings | Specifies that the clock-to-clock uncertainty applies only to falling edges of source clock list. Only one of the -from , -rise_from , or -fall_from arguments can be specified for the constraint to be valid. |
from_clock/rise_from_clock/fall_from_clock | list of strings | Specifies the list of clock names as the uncertainty source. |
to | list of strings | Specifies that the clock-to-clock uncertainty applies to both rising and falling edges of the destination clock list. Only one of the -to , -rise_to , or -fall_to arguments can be specified for the constraint to be valid. |
rise_to | list of strings | Specifies that the clock-to-clock uncertainty applies only to rising edges of the destination clock list. Only one of the -to , -rise_to , or -fall_to arguments can be specified for the constraint to be valid. |
fall_to | list of strings | Specifies that the clock-to-clock uncertainty applies only to falling edges of the destination clock list. Only one of the -to , -rise_to , or -fall_to arguments can be specified for the constraint to be valid. |
to_clock/rise_to_clock/fall_to_clock | list of strings | Specifies the list of clock names as the uncertainty destination. |
setup | None | Specifies that the uncertainty applies only to setup checks. If none or both -setup and -hold are present, the uncertainty applies to both setup and hold checks. |
hold | None | Specifies that the uncertainty applies only to hold checks. If none or both -setup and -hold are present, the uncertainty applies to both setup and hold checks. |
Return Type | Description |
---|---|
integer | Returns the ID of the clock uncertainty constraint. |
Supported Families
PolarFire® |
PolarFire SoC |
SmartFusion® 2 |
IGLOO® 2 |
RTG4™ |
Example
Simple Clock Uncertainty constraint examples.
The following example specifies uncertainty of 2 ns.
set_clock_uncertainty 2 [get_clocks clk]
The following example specifies setup uncertainty of 2 ns.
set_clock_uncertainty 2 -setup [get_clocks clk]
Clock to Clock Uncertainty constraint examples:
The following example specifies uncertainties of 10ns between Clk1 and Clk2 clock domains.
set_clock_uncertainty 10 -from [get_clocks { Clk1 }] -to [get_clocks { Clk2 }]
The following example specifies setup uncertainties between Clk1 and {Clk2 Clk3} clock domains with specific edges.
set_clock_uncertainty 0 -from [get_clocks { Clk1 }] -fall_to [get_clocks { Clk2 Clk3 }] -setup
set_clock_uncertainty 4.3 -fall_from [get_clocks { Clk1 Clk2 }] -rise_to *
set_clock_uncertainty 0.1 -rise_from [ get_clocks { Clk1 Clk2 }] \
-fall_to [get_clocks { Clk3 Clk4 }] -setup
set_clock_uncertainty 5 -rise_from [get_clocks {Clk1}] -to [ get_clocks {*} ]