3.6.2.4.10 SOC_CPU_MEM_BASE_ADDRESS

This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the base address of the memory window in the shared memory space (DDR) that can be accessed by the HLS module's AXI initiator interfaces. This address is used to configure the AXI interconnect that HLS modules connect to for accessing the shared memory.

Note that the value for the parameter is specified in hexadecimal format and must be prefixed with 0x.

Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.

Category
HLS Constraints
Value Type
Hexadecimal
Default Value (Based on Icicle SoC reference design)
0x80000000
Dependencies
None
Applicable Flows
SoC Flow Only
Test Status
Actively in-use
Examples
set_parameter SOC_CPU_MEM_BASE_ADDRESS 0x80000000