TCPIP_HTTP_NET_SSIVariableSet Function
C
bool TCPIP_HTTP_NET_SSIVariableSet(
const char* varName,
TCPIP_HTTP_DYN_ARG_TYPE varType,
const char* strValue,
int32_t intValue
);
Description
This function sets the new values for an SSI variable. If a variable with such name does not exist, it is created.
Preconditions
The HTTP module should have been initialized. SSI should be enabled.
Parameters
| Parameters | Description |
|---|---|
| varName | The SSI variable name. |
| varType | The type of the SSI variable. |
| strValue | Pointer to the string representation of the variable. |
| intValue | The integer value of the variable, if the type is integer. |
Returns
True - If the variable was updated or created successfully
False - The variable didn't exist and the attempt to create it failed (all slots already in use. Increase TCPIP_HTTP_NET_SSI_VARIABLES_NUMBER()).
Remarks
The string variable interpretation is needed even if the variable is of integer type. HTTP module will use that representation instead of doing a conversion to string of the intValue. The string representation should not exceed TCPIP_HTTP_NET_SSI_VARIABLE_STRING_MAX_LENGTH(). Any excess variables will be truncated.