TCPIP_HTTP_NET_SSIVariableDelete Function
C
bool TCPIP_HTTP_NET_SSIVariableDelete(
const char* varName
);
Description
This function deletes an SSI variable if it exists.
Preconditions
The HTTP module should have been initialized. SSI should be enabled.
Parameters
| Parameters | Description |
|---|---|
| varName | The SSI variable name. |
Returns
True - If the variable existed and was deleted.
False - The variable didn't exist.
Remarks
None.