TCPIP_HTTP_NET_ConnectionHasArgsSet Function
C
void TCPIP_HTTP_NET_ConnectionHasArgsSet(
TCPIP_HTTP_NET_CONN_HANDLE connHandle,
uint8_t args
);
Description
This function sets the value of the "cookies or get arguments" that are present.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| connHandle | HTTP connection handle. |
| args | Number of arguments. |
Returns
None.
Remarks
None.
Example
else if(!memcmp(filename, "cookies.htm", 11))
{
TCPIP_HTTP_NET_ConnectionHasArgsSet(connHandle, 1);
}