TCPIP_HTTP_NET_SSIVariableGet Function
C
const char* TCPIP_HTTP_NET_SSIVariableGet(
const char* varName,
TCPIP_HTTP_DYN_ARG_TYPE* pVarType,
int32_t* pVarInt
);
Description
This function performs a search for the corresponding SSI variable name and returns a pointer to the variable string representation.
Preconditions
The HTTP module should have been initialized. SSI should be enabled.
Parameters
| Parameters | Description |
|---|---|
| varName | The SSI variable to search for. |
| pVarType | Address to store the type of the SSI variable. |
| pVarInt | Address to store the integer value of this variable if the variable exists and is an integer, else this address won't be modified. Could be NULL if not needed. |
Returns
A valid pointer to the SSI variable string representation if the variable was found.
0 if there is no variable with such name.
Remarks
The returned value points to the internal SSI variable representation. This pointer should not be used for changing the SSI variable value.