TCPIP_HTTP_NET_ConnectionHasArgsSet Function
C
void TCPIP_HTTP_NET_ConnectionIsAuthorizedSet(
TCPIP_HTTP_NET_CONN_HANDLE connHandle,
uint8_t auth
);
Description
This function sets the authorization status for the current HTTP connection. This has to be one of the values in the set returned by the template_ConnectionFileAuthenticate() function.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| connHandle | HTTP connection handle. |
| auth | New authorization state. |
Returns
None.
Remarks
None.
Example
uint8_t auth = 0x80;
TCPIP_HTTP_NET_ConnectionIsAuthorizedSet(connHandle, auth);