TCPIP_HTTP_NET_ConnectionUserDataSet Function
C
void TCPIP_HTTP_NET_ConnectionUserDataSet(
TCPIP_HTTP_NET_CONN_HANDLE connHandle,
const void* uData
);
Description
This function will set the user data value for the current HTTP connection. This data belongs to the user and is not used in any way by the HTTP server module. It is available to the user by calling TCPIP_HTTP_NET_ConnectionUserDataGet().
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| connHandle | HTTP connection handle. |
| uData | User supplied data. |
Returns
None.
Remarks
None.
Example
uint32_t myConnData;
TCPIP_HTTP_NET_ConnectionUserDataSet(connHandle, (const void*)myConnData);