TCPIP_HTTP_NET_ConnectionHandleGet Function
C
TCPIP_HTTP_NET_CONN_HANDLE TCPIP_HTTP_NET_ConnectionHandleGet(
int connIx
);
Description
This function will return the connection handle of the requested HTTP connection index.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| connIx | The HTTP connection ix. |
Returns
A valid connection handle if the connection index is valid
0 if there is no such connection.
Remarks
None.
Example
TCPIP_HTTP_NET_CONN_HANDLE connHandle;
connHandle = TCPIP_HTTP_NET_ConnectionHandleGet(0);