TCPIP_HTTP_NET_SSIVariablesNumberGet Function
C
int TCPIP_HTTP_NET_SSIVariablesNumberGet(
int* pMaxNo
);
Description
This function returns the number of SSI variables that currently exist. It will also return the maximum number of variables that the SSI can hold.
Preconditions
The HTTP module should have been initialized. SSI should be enabled.
Parameters
| Parameters | Description |
|---|---|
| pMaxNo | Pointer to store the maximum number of SSI variables that can exist. Can be NULL if not needed. |
Returns
The number of current SSI variables that are in use.
Remarks
None.