TCPIP_HTTP_DYN_VAR_DCPT Structure
C
typedef struct {
const char* dynName;
const char* fileName;
uint16_t callbackID;
uint8_t dynFlags;
uint8_t nArgs;
TCPIP_HTTP_DYN_ARG_DCPT* dynArgs;
const void* dynContext;
} TCPIP_HTTP_DYN_VAR_DCPT;
Description
Data structure: TCPIP_HTTP_DYN_VAR_DCPT
This data type defines the structure of a HTTP dynamic variable descriptor. When the user registers a template_DynPrint() function for dynamic variable processing, this callback will receive the dynamic variable descriptor as a parameter.
Members
| Members | Description |
|---|---|
| dynName | ASCII string storing the dynamic variable name. |
| fileName | ASCII string storing the file name the dynamic variable belongs to. |
| callbackID | Callback ID: the dynamic variable index within the file. |
| dynFlags | A TCPIP_HTTP_DYN_VAR_FLAGS value. |
| nArgs | Number of arguments that the variable has. |
| dynArgs | Array of argument descriptors carrying the dynamic variable arguments. |
| dynContext | Dynamic context of the callback. This context is used by the HTTP server and is irrelevant to the user. Should NOT be modified in any way by the user. |
Remarks
None.