TCPIP_HTTP_NET_ConnectionDataBufferSizeGet Function
C
uint16_t TCPIP_HTTP_NET_ConnectionDataBufferSizeGet(
TCPIP_HTTP_NET_CONN_HANDLE connHandle
);
Description
This function returns the size of the HTTP connection internal data buffer.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| connHandle | HTTP connection handle. |
Returns
Size of the connection's general purpose data buffer.
Remarks
This is the parameter that was used for HTTP initialization in TCPIP_HTTP_NET_MODULE_CONFIG::dataLen.
Example
// Read a name
uint8_t* httpDataBuff = TCPIP_HTTP_NET_ConnectionDataBufferGet(connHandle);
uint16_t httpDataLen = TCPIP_HTTP_NET_ConnectionDataBufferSizeGet(connHandle);
if(TCPIP_HTTP_NET_ConnectionPostNameRead(connHandle, httpDataBuff, httpDataLen) == TCPIP_HTTP_NET_READ_INCOMPLETE)
{
return TCPIP_HTTP_NET_IO_RES_NEED_DATA;
}