| Macros | |
| TCPIP_HTTP_NET_CACHE_LEN | Max lifetime (sec) of static responses as string |
| TCPIP_HTTP_NET_CONFIG_FLAGS | Define the HTTP module configuration flags Use 0 for default See HTTP_MODULE_FLAGS definition for possible values |
| TCPIP_HTTP_NET_COOKIE_BUFFER_SIZE | Size of the buffer used for sending the cookies to the client. Should be able to accommodate the longest cookie response. Otherwise the cookies will be truncated. |
| TCPIP_HTTP_NET_DEFAULT_FILE | Indicate what HTTP file to serve when no specific one is requested |
| TCPIP_HTTP_NET_DYNVAR_ARG_MAX_NUMBER | maximum number of arguments for a dynamic variable |
| TCPIP_HTTP_NET_DYNVAR_DESCRIPTORS_NUMBER | how many buffers descriptors for dynamic variable processing they are independent of the HTTP connection number all the HTTP connections use from the dynamic descriptors pool |
| TCPIP_HTTP_NET_DYNVAR_MAX_LEN | maximum size for a complete dynamic variable: name + args must be <= TCPIP_HTTP_NET_FILE_PROCESS_BUFFER_SIZE! If it is much larger than needed then inefficiency occurs when reading data from the file and then discarding it because a much larger than needed data buffer was read |
| TCPIP_HTTP_NET_FILE_UPLOAD_ENABLE | Configure MPFS over HTTP updating Comment this line to disable updating via HTTP |
| TCPIP_HTTP_NET_FILE_UPLOAD_NAME | This is macro TCPIP_HTTP_NET_FILE_UPLOAD_NAME. |
| TCPIP_HTTP_NET_FIND_PEEK_BUFF_SIZE | Size of the peek buffer to perform searches into. If the underlying transport layer supports offset peak operation with a offset, the value could be smaller (80 characters, for example); otherwise, a one time peek is required and the buffer should be larger - recommended to be close to the size of the socket RX buffer. |
| TCPIP_HTTP_NET_MAX_CONNECTIONS | Maximum numbers of simultaneous supported HTTP connections. |
| TCPIP_HTTP_NET_MAX_DATA_LEN | Define the maximum data length for reading cookie and GET/POST arguments (bytes) |
| TCPIP_HTTP_NET_MAX_HEADER_LEN | The length of longest header string that can be parsed |
| TCPIP_HTTP_NET_MAX_RECURSE_LEVEL | The maximum depth of recursive calls for serving a web page: no dynvars files: 1; file including a file: 2 ; if the include file includes another file: +1 ; if a dyn variable: +1; Default value is 3; |
| TCPIP_HTTP_NET_RESPONSE_BUFFER_SIZE | Size of the buffer used for sending the response messages to the client. Should be able to accommodate the longest server response: Default setting should be 300 bytes |
| TCPIP_HTTP_NET_SKT_RX_BUFF_SIZE | Define the size of the RX buffer for the HTTP socket Use 0 for default TCP socket value The default recommended value for high throughput is > 2MSS (3 KB). The performance of a socket is highly dependent on the size of its buffers so it's a good idea to use as large as possible buffers for the sockets that need high throughput. |
| TCPIP_HTTP_NET_SKT_TX_BUFF_SIZE | Define the size of the TX buffer for the HTTP socket Use 0 for default TCP socket value The default recommended value for high throughput is > 2MSS (3 KB). The performance of a socket is highly dependent on the size of its buffers so it's a good idea to use as large as possible buffers for the sockets that need high throughput. |
| TCPIP_HTTP_NET_TASK_RATE | The HTTP task rate, ms The default value is 33 milliseconds. The lower the rate (higher the frequency) the higher the module priority and higher module performance can be obtained The value cannot be lower than the TCPIP_STACK_TICK_RATE. |
| TCPIP_HTTP_NET_TIMEOUT | Max time (sec) to await for more HTTP client data in an active connection state before timing out and disconnecting the socket |
| TCPIP_HTTP_NET_USE_AUTHENTICATION | Enable basic authentication support |
| TCPIP_HTTP_NET_USE_COOKIES | Enable cookie support |
| TCPIP_HTTP_NET_USE_POST | Define which HTTP modules to use If not using a specific module, comment it to save resources Enable POST support |
| TCPIP_HTTP_NET_CHUNK_RETRIES | retry limit for allocating a chunk from the pool If more retries are not successful the operation will be aborted |
| TCPIP_HTTP_NET_CHUNKS_NUMBER | number of chunks that are created It depends on the TCPIP_HTTP_NET_MAX_RECURSE_LEVEL and on the number of connections Maximum number should be TCPIP_HTTP_NET_MAX_CONNECTIONS * TCPIP_HTTP_NET_MAX_RECURSE_LEVEL i.e. TCPIP_HTTP_NET_MODULE_CONFIG::nConnections * TCPIP_HTTP_NET_MODULE_CONFIG::nChunks All the chunks are in a pool and are used by all connections |
| TCPIP_HTTP_NET_DYNVAR_PROCESS | This symbol enables the processing of dynamic variables Make it evaluate to false (0) if dynamic variables are not needed All the following symbols referring to dynamic variables are relevant only when TCPIP_HTTP_NET_DYNVAR_PROCESS != 0 |
| TCPIP_HTTP_NET_DYNVAR_PROCESS_RETRIES | retry limit for a dynamic variable processing ths puts a limit on the number of times a dynamic variable "dynamicPrint" function can return TCPIP_HTTP_DYN_PRINT_RES_AGAIN/TCPIP_HTTP_DYN_PRINT_RES_PROCESS_AGAIN and avoids having the HTTP code locked up forever. If more retries are attempted the processing will be considered done and dynamicPrint function will not be called again |
| TCPIP_HTTP_NET_FILE_PROCESS_BUFFER_RETRIES | Retry limit for allocating a file buffer from the pool. If more retries are not successful the operation will be aborted. |
| TCPIP_HTTP_NET_FILE_PROCESS_BUFFER_SIZE | Size of the buffer used for processing HTML, dynamic variable and binary files. For dynamic variable files it should be able to accommodate the longest HTML line size, including CRLF! |
| TCPIP_HTTP_NET_FILE_PROCESS_BUFFERS_NUMBER | Number of file buffers to be created; These buffers are used to store data while file processing is done They are organized in a pool Each file being processed needs a file buffer and tries to get it from the pool If a buffer is not available, the HTTP conenction will wait for one to become available. Once the file is done the file buffer is released and could be used by a different file The number depends on the number of files that are processed in parallel To avoid deadlock the number should be >= than the number of... more |
| TCPIP_HTTP_NET_FILENAME_MAX_LEN | maximum size of a HTTP file name with the path removed from the file name one extra char added for the string terminator |
| TCPIP_HTTP_NET_SSI_ATTRIBUTES_MAX_NUMBER | maximum number of attributes for a SSI command most SSI commands take just one attribute/value pair per line but multiple attribute/value pairs on the same line are allowed where it makes sense |
| TCPIP_HTTP_NET_SSI_CMD_MAX_LEN | maximum size for a SSI command line: command + attribute/value pairs must be <= TCPIP_HTTP_NET_FILE_PROCESS_BUFFER_SIZE! If it is much larger than needed then inefficiency occurs when reading data from the file and then discarding it because a much larger than needed data buffer was read |
| TCPIP_HTTP_NET_SSI_ECHO_NOT_FOUND_MESSAGE | message to echo when echoing a not found variable |
| TCPIP_HTTP_NET_SSI_PROCESS | This symbol enables the processing of SSI commands Make it evaluate to false (0) if SSI commands are not needed All the following symbols referring to SSI commands are relevant only when TCPIP_HTTP_NET_SSI_PROCESS != 0 |
| TCPIP_HTTP_NET_SSI_STATIC_ATTTRIB_NUMBER | number of static attributes associated to a SSI command if the command has more attributes than this number the excess will be allocated dynamically |
| TCPIP_HTTP_NET_SSI_VARIABLE_NAME_MAX_LENGTH | maximum length of a SSI variable name any excess characters will be truncated Note that this can result in multiple variables being represented as one SSI variable |
| TCPIP_HTTP_NET_SSI_VARIABLE_STRING_MAX_LENGTH | maximum size of a SSI string variable value any excess characters will be truncated Note that the variable value requires SSI storage that's allocated dynamically Also, this value determines the size of an automatic (stack) buffer when the variable is echoed. If this value is large, make sure you have enough stack space. |
| TCPIP_HTTP_NET_SSI_VARIABLES_NUMBER | maximum number of SSI variables that can be created at run time These variables are stored in an internal hash. For max. efficiency this number should be a prime. |
| TCPIP_HTTP_NET_CONNECTION_TIMEOUT | Persistent connection idle timeout, in seconds If a persistent connection is idle for more that this timeout the server will close it. Usually the client closes the connection. Using this timeout value the server can close the its side of the connection to avoid all connections to remain indefinitely open if the client misbehaves. Use 0 to never timeout. The timeout value has to be <= 32767 seconds. |
| HTTP_NET_CONFIG_H | This is macro HTTP_NET_CONFIG_H. |
| TCPIP_HTTP_NET_FREE_FUNC | HTTP corresponding deallocation function, free style This is the function the HTTP will call for freeing the allocated memory Use standard C library 'free' or 0 as a default If it's 0, HTTP will use the allocation functions passed in at the stack initialization |
| TCPIP_HTTP_NET_MALLOC_FUNC | HTTP allocation function, malloc style This is the function the HTTP will call to allocate memory needed for: dynamic variables, SSI or file uploads. Use standard C library 'malloc' or 0 as a default If it's 0, HTTP will use the allocation functions passed in at the stack initialization |
| Functions | |
| TCPIP_HTTP_NET_ConnectionByteCountDec | Decrements the connection byte count. |
| TCPIP_HTTP_NET_ConnectionByteCountSet | Sets how many bytes are available to be read. |
| TCPIP_HTTP_NET_ConnectionCallbackPosSet | Sets the callback position indicator. |
| TCPIP_HTTP_NET_ConnectionDiscard | Discards any pending data in the connection RX buffer. |
| TCPIP_HTTP_NET_ConnectionFlush | Immediately transmits all connection pending TX data. |
| TCPIP_HTTP_NET_ConnectionHasArgsSet | Sets whether there are get or cookie arguments. |
| TCPIP_HTTP_NET_ConnectionIsAuthorizedSet | Sets the authorized state for the current connection. |
| TCPIP_HTTP_NET_ConnectionNetHandle | Returns the network handle of the current connection. |
| TCPIP_HTTP_NET_ConnectionPeek | Reads a specified number of data bytes from the connection RX buffer without removing them from the buffer. |
| TCPIP_HTTP_NET_ConnectionPostSmSet | Set the POST state machine state. |
| TCPIP_HTTP_NET_ConnectionRead | Reads an array of data bytes from a connection's RX buffer. |
| TCPIP_HTTP_NET_ConnectionReadBufferSize | Returns the size of the connection RX buffer. |
| TCPIP_HTTP_NET_ConnectionReadIsReady | Determines how many bytes can be read from the connection RX buffer. |
| TCPIP_HTTP_NET_ConnectionStatusSet | Sets HTTP status. |
| TCPIP_HTTP_NET_ConnectionStringFind | Helper to find a string of characters in an incoming connection buffer. |
| TCPIP_HTTP_NET_ConnectionUserDataSet | Sets the user data parameter for the current connection. |
| TCPIP_HTTP_NET_DynamicWrite | Writes a data buffer to the current connection |
| TCPIP_HTTP_NET_DynamicWriteString | Helper for writing a string within a dynamic variable context. |
| TCPIP_HTTP_NET_Task | Standard TCP/IP stack module task function. |
| TCPIP_HTTP_NET_URLDecode | Parses a string from URL encoding to plain text. |
| TCPIP_HTTP_NET_UserHandlerDeregister | Deregisters a previously registered HTTP user handler. |
| TCPIP_HTTP_NET_UserHandlerRegister | Registers a user callback structure with the HTTP server |
| TCPIP_HTTP_NET_ActiveConnectionCountGet | Gets the number of active (and inactive) connections. |
| TCPIP_HTTP_NET_ArgGet | Locates a form field value in a given data array. |
| TCPIP_HTTP_NET_ConnectionByteCountGet | Returns how many bytes are available to be read. |
| TCPIP_HTTP_NET_ConnectionCallbackPosGet | Returns the callback position indicator. |
| TCPIP_HTTP_NET_ConnectionDataBufferGet | Returns pointer to connection general purpose data buffer. |
| TCPIP_HTTP_NET_ConnectionFileGet | Get handle to current connection's file. |
| TCPIP_HTTP_NET_ConnectionHasArgsGet | Checks whether there are get or cookie arguments. |
| TCPIP_HTTP_NET_ConnectionIsAuthorizedGet | Gets the authorized state for the current connection. |
| TCPIP_HTTP_NET_ConnectionPostSmGet | Get the POST state machine state. |
| TCPIP_HTTP_NET_ConnectionSocketGet | Get the socket for the current connection. |
| TCPIP_HTTP_NET_ConnectionStatusGet | Gets HTTP status. |
| TCPIP_HTTP_NET_ConnectionUserDataGet | Gets the user data parameter for the current connection. |
| TCPIP_HTTP_NET_ConnectionPostNameRead | Reads a name from a URL encoded string in the network transport buffer. |
| TCPIP_HTTP_NET_ConnectionPostValueRead | Reads a value from a URL encoded string in the network transport buffer. |
| TCPIP_HTTP_NET_ConnectionDataBufferSizeGet | Returns the size of the connection general purpose data buffer. |
| TCPIP_HTTP_NET_ConnectionDynamicDescriptors | Returns the number of dynamic variable descriptors |
| TCPIP_HTTP_NET_SSIVariableDelete | Function to delete an SSI variable. |
| TCPIP_HTTP_NET_SSIVariableGet | Function to get access to an existing SSI variable. |
| TCPIP_HTTP_NET_SSIVariableGetByIndex | Function to get access to an existing SSI variable. |
| TCPIP_HTTP_NET_SSIVariableSet | Function to set an SSI variable. |
| TCPIP_HTTP_NET_SSIVariablesNumberGet | Function to get the number of the current SSI variables. |
| TCPIP_HTTP_NET_ConnectionHandleGet | Gets the connection handle of a HTTP connection. |
| TCPIP_HTTP_NET_ConnectionIndexGet | Gets the index of the HTTP connection. |
| TCPIP_HTTP_NET_DynamicFileInclude | Dynamically includes/writes a file to the HTTP connection. |
| Data Types and Constants | |
| _tag_TCPIP_HTTP_NET_USER_CALLBACK | HTTP user implemented callback data structure. |
| TCPIP_HTTP_DYN_ARG_DCPT | HTTP dynamic argument descriptor. |
| TCPIP_HTTP_DYN_ARG_TYPE | HTTP supported dynamic variables argument types. |
| TCPIP_HTTP_DYN_PRINT_RES | Dynamic print result when a dynamic variable print callback function returns; |
| TCPIP_HTTP_DYN_VAR_DCPT | HTTP dynamic variable descriptor. |
| TCPIP_HTTP_DYN_VAR_FLAGS | HTTP supported dynamic variables flags. |
| TCPIP_HTTP_NET_CONN_HANDLE | HTTP connection identifier, handle of a HTTP connection |
| TCPIP_HTTP_NET_EVENT_TYPE | HTTP reported run-time events. |
| TCPIP_HTTP_NET_IO_RESULT | Result states for execution callbacks |
| TCPIP_HTTP_NET_MODULE_CONFIG | HTTP module dynamic configuration data |
| TCPIP_HTTP_NET_MODULE_FLAGS | HTTP module configuration flags Multiple flags can be OR-ed |
| TCPIP_HTTP_NET_READ_STATUS | Result states for TCPIP_HTTP_NET_ConnectionPostNameRead, TCPIP_HTTP_NET_ConnectionPostValueRead and TCPIP_HTTP_NET_ConnectionPostReadPair |
| TCPIP_HTTP_NET_STATUS | Supported Commands and Server Response Codes |
| TCPIP_HTTP_NET_USER_CALLBACK | HTTP user implemented callback data structure. |
| TCPIP_HTTP_NET_USER_HANDLE | HTTP user handle. |
| TCPIP_HTTP_NET_ConnectionPostReadPair | Reads a name and value pair from a URL encoded string in the network transport buffer. |
| TCPIP_HTTP_SSI_ATTR_DCPT | HTTP SSI attribute descriptor. |
| TCPIP_HTTP_SSI_NOTIFY_DCPT | HTTP SSI notification descriptor. |
| _HTTP_NET_H | This is macro _HTTP_NET_H. |