TCPIP_SNMP_IsValidLength Function
C
bool TCPIP_SNMP_IsValidLength(
SNMP_ID var,
uint8_t len,
uint8_t index
);
Description
This function is used to validate the dynamic variable data length to the variable data type. It is called before the SET request is processed. This is a callback function called by module. User application must implement this function.
Preconditions
TCPIP_SNMP_ProcessSetVar() is called.
Parameters
| Parameters | Description |
|---|---|
| var | Variable id whose value is to be set. |
| len | Length value that is to be validated. |
Returns
True - If given var can be set to given len.
False - If the given var cannot be set to the given len.
Remarks
This function will be called for only dynamic variables that are defined as ASCII_STRING and OCTET_STRING.