TCPIP_SNMP_TrapSpecificNotificationSet Function
C
void TCPIP_SNMP_TrapSpecificNotificationSet(
uint8_t specTrap,
uint8_t genTrap,
SNMP_ID trapID
);
Description
The SNMP user needs to call this function before transmitting any traps. This function will set the vendor specific trap, generic trap, and default trap ID value. The SNMPv2 trap will use this trap ID while sending a specific trap.
Preconditions
TCPIP_SNMP_Initialize() is already called.
Parameters
| Parameters | Description |
|---|---|
| specTrap | Vendor specific trap value (enumeration value of SNMP_VENDOR_SPECIFIC_TRAP_NOTIFICATION_TYPE). |
| genTrap | Generic trap (enumeration value of SNMP_GENERIC_TRAP_NOTIFICATION_TYPE). |
| trapID | Trap ID. |
Returns
None.
Remarks
The Trap ID is the NOTIFICATION-TYPE of the ASN.1 MIB format. From the Trap ID, the SNMP agent will be able to obtain the OID string, which will be used while preparing TRAPv2 second varbind.