TCPIP_SNMP_MibIDSet Function
C
void TCPIP_SNMP_MibIDSet(
uint32_t mibID
);
Description
This function is used to Set the MIB ID which is require while transmitting SNMP notification.SNMP user can this function without adding this to the Microchip MIB script.
Preconditions
TCPIP_SNMP_Initialize() is already called.
Parameters
| Parameters | Description |
|---|---|
| mibID | Trap client MIB ID. |
Returns
None.
Remarks
None.