TCPIP_SNMP_WriteCommunityGet Function
C
bool TCPIP_SNMP_WriteCommunityGet(
int index,
int len,
uint8_t * dest
);
Description
This function is used to collect WRITE community string from the global community table with respect to the index value.
Preconditions
TCPIP_SNMP_Initialize() is already called.
Parameters
| Parameters | Description |
|---|---|
| index | One of the index of community table and it should be less than TCPIP_SNMP_MAX_COMMUNITY_SUPPORT. |
| len | Length of the community string expected. It should not be more than TCPIP_SNMP_COMMUNITY_MAX_LEN. |
| dest | Copy the community string to this address and it should have a valid address. |
Returns
True - If the community string is collected.
False - If the community string is not collected.
Remarks
None.