Bits 31:0 – ADCCNTB[31:0] Analog-to-Digital
Count Base Address bits
The ADCCNTB register
contains the user-defined RAM address at which the DMA engine will start saving the
current count of output samples (if the DMACNTEN bit (ADCDMASTAT[15]) is set), which
is already written to each of the buffers in the System RAM for each ADC core. The ADCx core will have its Buffer A current
sample count saved at the address ((ADCCNTB) + (2 × x)) and its Buffer B current
sample count saved at the address ((ADCCNTB) + (2 × (x + 1))). Where ‘x’ is the
dedicated ADC core ID.