14.24.3 Projects Window – File Menu
Right click on a file name in the Projects window to pop up the File menu. The table below shows the specific menu items.
| Menu Item | Description |
|---|---|
| Open | Opens this file in a tabbed Editor window. |
| Cut | Removes the file from the project, but places a copy of it on the clipboard. |
| Copy | Places a copy of the file on the clipboard. |
| Paste | To paste the clipboard copy of a file into the project. |
| Exclude file(s) from current configuration | Select a file
or files to exclude from the current project configuration. Once a file
has been excluded, right clicking on it again will show
Include file(s) from the current
configuration. The same as opening the Project Properties window, selecting File Inclusion/Exclusion and including/excluding the file. |
| Compile File | Compiles only the current file. |
| Remove from Project | Removes the
file from the project. This does not delete the file from the PC. To delete the file from the project and the computer, use the Delete key. |
| Rename | Renames the file. |
| Save as Template | Saves the current file as a template file. |
| History | To view, or revert to, the local history for the file. |
| Tools | File tools
include:
|
| Properties | Sets file
properties differently from the project properties. Select to exclude the file from the build or override the project build options by selecting a different configuration. |