14.24.2 Projects Window – Project Menu
Right click on a project name in the Projects window to pop up the Project menu. Menu items are shown in the tables below.
| Menu Item | Description |
|---|---|
| Build | Builds the
project according to the options selected in the Project
Properties window. Note: When you
Debug or Run, your
project is built automatically. |
| Clean and Build | Cleans and
then builds the project according to the options selected in the
Project Properties window. Note: When you
Debug or Run, your
project is built automatically. |
| Clean | Cleans the project by deleting the outputs of previous builds. |
| Batch Build | Builds one or more configurations. |
| Set Configuration | Displays project configurations for selection, or click Customize to open the Project Properties window to manage project configurations. |
| New | Creates a new
item
for MPLAB X IDE; embedded file types are
available. See New Submenu Items table below. |
| Add | Adds an item
for MPLAB X IDE; embedded file types are
available. See Add Submenu Items table below. |
| Set as Main Project | Sets this
project as the main project. This is useful when you are working with multiple projects. |
| Find | Finds specific text in files in this project. |
| Locate Headers | Locates all
the header files (.h) called out in the C code
project files and presents them in a checklist window so they may be
added to the project There are several reasons why you might want to add headers to your project:
This feature is able to locate user-generated header files for all Microchip toolchains. |
| Run | Executes the project code. |
| Debug | Executes the project code in a debug environment. |
| Step Into | Steps into Paused code running in the debug environment. |
| Make and Program Device | Programs the target device and holds in Reset (do not run). |
| Projects | Select Project actions. See Projects Submenu Items table below. |
| Close | Closes the selected project. |
| Open Required Projects | Loads all other projects that are required for the selected project to run. |
| Code Assistance | Selects assistance in creating code: code folding, code completion, etc. |
| Analysis | Displays list of analysis tools for selection. |
| Show Code Coverage Summary | Opens Code Coverage window to display summary. |
| Versioning | Controls the version of the project by using a version control system. |
| History | To view, or revert to, the local history for the project. |
| Properties | Sets project
properties. For MPLAB X IDE, the Project Properties window is specific to embedded development. |
| Menu Item | Description |
|---|---|
| Directory | Opens the New Directory dialog. To view the new directory, see the Files window. Note: To create a new logical folder, select . |
| Compiler-specific header file | Click to create the compiler-specific header file template. For example, xc32_header.h. |
| Compiler-specific file | Click to create the compiler-specific file template. For example, xc32_newfile.c. |
| Text File | Opens the New Text File dialog. |
| Other | Opens the New File dialog. |
| Menu Item | Description |
|---|---|
| Add Existing Item | Adds an existing file to
the project. The path to the file may be auto (selected by MPLAB X IDE), absolute or relative. Additionally, you may choose to copy the file into the project folder. |
| Add Existing Items from Folders | Adds all files contained
in the specified folder(s). You may also specify a pattern to ignore certain folders from inclusion. Click Default to see the default pattern. See also , Files ignored by the IDE. |
| Add Logical Folder | Adds a new logical folder
to the Projects tree. Note: To
create an actual folder, select . To view the new directory, see the Files window. |
| Add External Item | Adds an existing item to
the project. The path to the file may be auto (selected by MPLAB X IDE), absolute or relative. Additionally, you may choose to copy the file into the project folder. This is useful for adding simulator files, data sheet PDFs, and other files to the project for your reference. |
| Add autoload.py | Adds the autoload.py file to support scripting for devices supporting this feature. |
| Learn more about scripting | Opens the WebHelp topic Use IDE Scripting (autoload.py). |
| Menu Item | Description |
|---|---|
| Package | Packages the current project into a .zip file. |
| Rename | Renames the project. |
| Move | Moves the project to
another location. Along with the project, it moves the source files that are inside the project directory. Files outside the project directory are not moved. However, the project still maintains reference to the files outside the project directory – this is by design. |
| Copy | Creates a copy of the
project. If the source files are within the project directory, the source files are also copied to the new location. Files outside the project directory are not copied. However, the project still maintains reference to the files outside the project directory – this is by design. |
| Delete | Deletes the project
files. The project file is deleted but not the contents under the project directory. Only on selecting Also delete sources are all the source files deleted. |
| Export Hex | Exports the project build
as a Hex file. In MPLAB IDE v8, export is an extraction of memory objects. In MPLAB X IDE, export is the hex file result of a build; therefore, it needs to include all necessary auxiliary memory settings for configuration and EEPROM in code. If analyzing the exported hex file, use the device PIC file to decode extended linear address records. |