14.24.4 Projects Window – Window Menu
Right click in an empty area in the Projects window to pop up the Window menu. The table below shows the specific menu items.
| Menu Item | Description |
|---|---|
| New Project | Launches the New Project wizard. |
| New File | Launches the New File wizard. |
| Open Project | Opens an existing project. |
| Open Recent Project | Opens an existing project for the list of recent projects. |
| Project Groups | Opens the Manage Groups dialog to select, create, remove or view project groups. |
| Build Project Name* | Builds the selected project shown in parentheses. |
| Clean and Build Project Name* | Cleans and Builds the selected project shown in parentheses. |
| Set Main Project | Sets the main project from the list of open projects. |
| Collapse All | Collapses all tree items. |
| Show Selected Node(s) Project Owner | See NetBeans Help, Projects Window. |
| * Either name of project or “Main Project” | |