14.17.6 Data Flash Memory
The Data Flash Memory window displays locations in the range of data flash memory for the currently selected 32-bit device.

Data Flash Memory Display
When using a hardware tool for debug, some registers may show an R for each nibble of data to represent a reserved resource.
Data Flash Memory Format
This window will have the following columns:
- Address – Hexadecimal address of the data in the next column.
- Data Blocks – Hexadecimal data, shown in 4-byte blocks.
- ASCII – ASCII representation of the corresponding line of data.
Data Flash Memory Window Icons
Icons are located on the left side of the window.
| Icon | Icon Text | Function |
|---|---|---|
![]() | Find | Specify a string to find in the window. Select to match whole word or case. |
![]() | Find Next | Find next instance of string from Find. |
![]() | Find Previous | Find previous instance of string from Find. |
![]() | Go To | Go to specified line number or address. |
Data Flash Memory Window Menu
Right click in the memory window data area to pop up this menu. Not all items may be visible for all 32-bit MCUs.
| Item | Description |
|---|---|
| Hex Width Display | Data Format
Only Set the hexadecimal display width. (Options depend on the device selected). Example: One byte, e.g., 00 01 02 ... 0E 0F Two bytes, e.g., 00 02 04 ... 0C 0E Four bytes, e.g., 00 04 08 0C |
| Fill Memory | Fill memory from
Start Address to End
Address with the value in
Data. Specify other options in the Fill Memory dialog. |
| Go To | Go to the address/function specified using the Go To dialog. |
| Find | Find text specified using the Find dialog. |
| Output To File | Write the displayed window contents to a text file using the Output to File dialog. |
| Import Table | Import tabular data from a file into a Memory window using the Import Table dialog. |
| Export Table | Export tabular data from a Memory window into a file using the Export Table dialog. |
| Print the contents of this
window using the Print dialog. Note: If you have a
large memory device, the number of pages printed can become very
large. A suggestion is to print the window contents to a file
(Print dialog,
General tab, Print to
File check box) and then select which pages from
the file you need to print. | |
| Adjust Table Columns | Adjust the columns automatically. |