38 Instruction Set Summary
The dsPIC33AK512MPS512 family of devices supports modified Harvard architecture. For details of the 32-bit Comprehensive Instruction Set for the dsPIC33AK512MPS512 device family, refer to the “dsPIC33A Programmer's Reference Manual” (DS70005540).
The instruction set is highly orthogonal and is grouped into five basic categories:
- Long word, word or byte-oriented operations
- Bit-oriented operations
- Literal operations
- DSP operations
- Control operations
Table 38-1 lists the general symbols used in describing the instructions.
The instruction set summary in Table 38-2 lists all the instructions, along with the status flags affected by each instruction.
Most long word, word or byte-oriented operations’ W register instructions (including barrel shift instructions) have three operands:
- The first source operand, which is typically a register ‘Wb’ without any address modifier.
- The second source operand, which is typically a register ‘Ws’ with or without an address modifier.
- The destination of the result, which is typically a register ‘Wd’ with or without an address modifier.
However, long word, word or byte-oriented operations’ file register instructions have two operands:
- The file register specified by the value ‘f’.
- The destination, which could be either the file register ‘f’ or any W register.
Most bit-oriented instructions (including simple rotate/shift instructions) have two operands:
- The W register (with or without an address modifier) or file register (specified by the value of ‘Ws’ or ‘f’)
- The bit in the W register or file register (specified by a literal value or indirectly by the contents of register ‘Wb’)
The literal instructions that involve data movement can use some of the following operands:
- A literal value to be loaded into a W register (specified by ‘k’).
- The W register or file register where the literal value is to be loaded (specified by ‘Wb’ or ‘f’).
However, literal instructions that involve arithmetic or logical operations use some of the following operands:
- The first source operand, which is a register ‘Wb’ without any address modifier.
- The second source operand, which is a literal value.
- The destination of the result (only if not the same as the first source operand), which is typically a register ‘Wd’ with or without an address modifier.
The MAC class of DSP instructions can use some of the
following operands:
- The accumulator (A or B) to be used (required operand)
- The W registers to be used as the two operands
- The X and Y address space prefetch operations
- The X and Y address space prefetch destinations
- The accumulator write-back destination
The other DSP instructions do not involve any multiplication and can include:
- The accumulator to be used (required)
- The source or destination operand (designated as Wso or Wdo, respectively) with or without an address modifier
- The amount of shift specified by a W register ‘Wn’ or a literal value.
The control instructions can use a program memory address.
Most single-word instructions are executed in a single instruction cycle
unless a conditional test is true. The Program Counter is changed as a result of the
instruction. In these cases, the execution takes multiple instruction cycles with the
additional instruction cycle(s) executed as a NOP. Certain instructions
that involve skipping over the subsequent instruction require extra cycles if the skip is
performed, depending on whether the instruction being skipped is a single-word or two-word
instruction.
| Symbol(1) | Description |
|---|---|
{ } | Optional field or operation |
[text] | The location addressed by text |
(text) | The contents of text |
#text | The literal defined by text |
{label:} | Optional label name |
[n:m] | Register bit field |
.l | 32-bit Long Word mode selection |
.b | 8-bit Byte mode selection |
.sl | 24-bit (literal) Word mode selection |
.V | Destination data value select (MAXABW, MINABW and FLIMW) |
.w | 16-bit Word mode selection (default) |
AWB | Accumulator write back destination address register |
bit3 | 3-bit bit selection field (used in byte addressed instructions) (0:7) |
bit4 | 4-bit bit selection field (used in word addressed instructions) (0:15) |
| C, N, OV, Z | ALU status bits: Carry, Digit Carry, Negative, Overflow and Zero |
| d | File register destination (W0, none) |
Expr | Absolute address, label or expression (resolved by the linker) |
f | File register address (0x0000:0xFFFF) or (0x00000:0xFFFFF) (addressable space varies depending upon instruction class) |
Fd(2) | One of 32 FPU destination data registers (F0:F31) (Register Direct) |
Fs(2) | One of 32 FPU source data registers (F0:F31) (Register Direct) |
FSR, FSRH,
FCR, FEAR 1(2) | FPU special (control & status) coprocessor registers (Register Direct) |
label | Translates to a literal representing the location of the label name |
lit1 | 1-bit unsigned literal (0:1) |
lit3 | 3-bit unsigned literal (0:7) |
lit5 | 5-bit unsigned literal (0:31) |
lit6 | 6-bit unsigned literal (0:63) |
lit8 | 8-bit unsigned literal (0:255) |
lit16 | 16-bit unsigned literal (0:65535) |
lit24 | 24-bit unsigned literal (0:1677215; LSb must
be 0 if an address) |
lit32 | 32-bit unsigned literal (0:4294967295) |
none | Field does not require an entry and may be blank |
OA, OB, SA,
SB | DSC status bits: ACCA Overflow, ACCB Overflow, ACCA Saturate and ACCB Saturate |
PC | Program Counter |
Rdo | Destination Working register |
Rnd | Instruction rounding mode [E, Z, P, N] |
Rso | Source Working register |
Slit6 | Signed 6-bit literal (-32:31) |
Slit7 | Signed 7-bit literal (-64:63) |
Slit8 | Signed 8-bit literal (-128:127) |
Slit20 | Signed 20-bit literal (-524288:524287) |
SR | Status register |
text1
∈ {text2,
{text3,…} | text1 must be in the set of
text2, text3, ... |
| v | Selects MULxxx operand data types |
Wb | Base Working register |
Wd | Destination Working register |
Wm | One of 16 Working registers (W0:W15) |
Wn | Both source and destination Working register (W0:W15) |
Wnd | One of 16 destination Working registers |
Wns | One of 16 source Working registers |
Wm *
Wm | Multiplicand and Multiplier Working register for Square instructions |
Wm *
Wn | Multiplicand and Multiplier W register for DSP instructions |
Ws | Source Working register |
Wx | X data space fetch address register for DSP instructions |
Wy | Y data space fetch address register for DSP instructions |
|
Note:
| |
| Base Instr # | Assembly Mnemonic | Assembly Syntax | Description | # of Words | # of Cycles(1) | Status Flags Affected |
|---|---|---|---|---|---|---|
| 1 | ABS | ABS Fs, Fd | Absolute value of Fs (FPU Instr) | 1 | 1 | SUBO |
| 2 | ADD | ADD A | Add Accumulators | 0.5 | 1 | OA, SA, OB, SB |
| ADD Rso,#Slit6, A | 16-bit Signed Add to Accumulator | 1 | 1 | OA, SA, OB, SB | ||
| ADD f,Wn | f = f + Wn | 1 | 1 | C, N, OV, Z | ||
| ADD f,Wn,Wn | Wn = f + Wn | 1 | 1 | C, N, OV, Z | ||
| ADD.l #lit5,Wn | Wn = Wn + lit5 | 0.5 | 1 | C, N, OV, Z | ||
| ADD #lit16,Wn | Wn = Wn + lit16 | 0.5/1 | 1 | C, N, OV, Z | ||
| ADD Wb,Ws,Wd | Wd = Wb + Ws | 1 | 1 | C, N, OV, Z | ||
| ADD Wb,#lit7,Wd | Wd = Wb + lit7 (literal zero-extended) | 1 | 1 | C, N, OV, Z | ||
| ADD Fb, Fs, Fd | Fd = Fb + Fs (FPU Instr) | SUBO, INX, UDF, OVF, INVAL | ||||
| 3 | ADDC | ADDC f,Wn | f = f + Wn + (C) | 1 | 1 | C, N, OV, Z |
| ADDC f,Wn,Wn | Wn = f + Wn + (C) | 1 | 1 | C, N, OV, Z | ||
| ADDC #lit16,Wn | Wn = Wn + lit16 + (C) | 1 | 1 | C, N, OV, Z | ||
| ADDC Wb,Ws,Wd | Wd = Wb + Ws + (C) | 0.5/1 | 1 | C, N, OV, Z | ||
| ADDC Wb,#lit7,Wd | Wd = Wb + lit7 + (C)(literal zero-extended) | 1 | 1 | C, N, OV, Z | ||
| 4 | AND | AND f,Wn | f = f .AND. Wn | 1 | 1 | N, Z |
| AND f,Wn,Wn | W0 = f .AND. Wn | 1 | 1 | N, Z | ||
| AND #lit16,Wn | Wn = Wn .AND. lit16 | 1 | 1 | N, Z | ||
| AND Wb,Ws,Wd | Wd = Wb .AND. Ws | 0.5/1 | 1 | N, Z | ||
| AND Wb,#lit7,Wd | Wd = Wb .AND. Lit7 (literal zero-extended) | 1 | 1 | N, Z | ||
| AND1 Wb,#lit7,Wd | Wd = Wb .AND. Lit7 (literal zero-extended) | 1 | 1 | N, Z | ||
| AND #lit16, FSR | FSR = FSR AND lit16 (FPU instr) | 1 | 1 | SUBO, HUGI, INX, UDF, OVF, DIV0, INVAL | ||
| AND #lit16, FCR | FCR = FCR AND lit16 (FPU instr) | 1 | 1 | None | ||
| AND #lit16, FEAR | FEAR = FEAR AND lit16 (FPU instr) | 1 | 1 | None | ||
| 5 | ASR | ASR f | f = Arithmetic Right Shift f by 1 | 1 | 1 | N, Z |
| ASR f,Wn | Wn = Arithmetic Right Shift f by 1 | 1 | 1 | N, Z | ||
| ASR Ws,Wd | Wd = Arithmetic Right Shift Ws by 1 | 0.5/1 | 1 | N, Z | ||
| ASR Ws,Wb,Wd | Wnd = Arithmetic Right Shift Ws by Wb | 0.5/1 | 1 | N, Z | ||
| ASR Ws,lit5,Wd | Wnd = Arithmetic Right Shift Ws by lit5 | 0.5/1 | 1 | N, Z | ||
| 6 | ASRM | ASRM Ws, #lit5, Wnd | Wnd = Arithmetic Right Shift Ws by lit5, then logically OR with next lsw | 1 | 2 | N, Z |
| ASRM Ws, Wb, Wnd | Wnd = Arithmetic Right Shift Ws by Wb, then logically OR with next lsw | 1 | 2 | N, Z | ||
| 7 | BCLR | BCLR.b f,bit3 | Bit Clear f | 1 | 1 | None |
| BCLR Ws,bit4 | Bit Clear Ws | 0.5/1 | 1 | None | ||
| 8 | BFEXT | BFEXT bit4,wid5,Ws,Wb | Bit Field Extract from Ws to Wb | 1 | 1 | None |
| BFEXT bit4,wid5,f,Wb | Bit Field Extract from f to Wb | 2 | 2 | None | ||
| 9 | BFINS | BFINS bit4,wid5,Wb,Ws | Bit Field Insert from Wb into Ws | 1 | 1 | None |
| BFINS bit4,wid5,Wb,f | Bit Field Insert from Wb into f | 2 | 2 | None | ||
| BFINS bit4,wid5,#lit8,Ws | Bit Field Insert lit8 into Ws | 2 | 2 | None | ||
| 10 | BOOTSWP | BOOTSWP | Swap the Active and Inactive Program Flash Space | 1 | 2 | None |
| 11 | BRA | BRA Label | Branch Unconditionally | 1 | 1 | None |
| BRA Wn | Computed Branch | 1 | 2 | None | ||
| BRA C,Label | Branch if Carry | 1 | 1(2/3) | None | ||
| BRA GE,Label | Branch if greater than or equal | 1 | 1(2/3) | None | ||
| BRA GEU,Label | Branch if unsigned greater than or equal | 1 | 1(2/3) | None | ||
| BRA GT,Label | Branch if greater than | 1 | 1(2/3) | None | ||
| BRA GTU,Label | Branch if unsigned greater than | 1 | 1(2/3) | None | ||
| BRA LE,Label | Branch if less than or equal | 1 | 1(2/3) | None | ||
| BRA LEU,Label | Branch if unsigned less than or equal | 1 | 1(2/3) | None | ||
| BRA LT,Label | Branch if less than | 1 | 1(2/3) | None | ||
| BRA LTU,Label | Branch if unsigned less than | 1 | 1(2/3) | None | ||
| BRA N,Label | Branch if Negative | 1 | 1(2/3) | None | ||
| BRA NC,Label | Branch if Not Carry | 1 | 1(2/3) | None | ||
| BRA NN,Label | Branch if Not Negative | 1 | 1(2/3) | None | ||
| BRA NOV,Label | Branch if Not Overflow | 1 | 1(2/3) | None | ||
| BRA NZ,Label | Branch if Not Zero | 1 | 1(2/3) | None | ||
| BRA Z,Label | Branch if Zero | 1 | 1(2/3) | None | ||
| BRA OA,Label | Branch if accumulator A overflow | 1 | 1(2/3) | None | ||
| BRA OB,Label | Branch if accumulator B overflow | 1 | 1(2/3) | None | ||
| BRA OV,Label | Branch if Overflow | 1 | 1(2/3) | None | ||
| BRA SA,Label | Branch if accumulator A saturated | 1 | 1(2/3) | None | ||
| BRA SB,Label | Branch if accumulator B saturated | 1 | 1(2/3) | None | ||
| 12 | BREAK | BREAK | Stop User Code Execution | 1 | 1 | None |
| 13 | BSET | BSET.b f,bit3 | Bit Set f | 1 | 1 | None |
| BSET Ws,bit4 | Bit Set Ws | 0.5/1 | 1 | None | ||
| 14 | BSW | BSW.C Ws,Wb | Write C or Z bit to Ws<Wb> | 1 | 1 | None |
| BSW.Z Ws,Wb | Write C or Z bit to Ws<Wb> | 0.5/1 | 1 | None | ||
| 15 | BTG | BTG.b f,bit3 | Bit Toggle f | 1 | 1 | None |
| BTG Ws,bit4 | Bit Toggle Ws | 0.5/1 | 1 | None | ||
| 16 | BTSC | Not supported | N/A | |||
| 17 | BTSS | Not supported | N/A | |||
| 18 | BTST | BTST.b f,bit3 | Bit Test f | 1 | 1 | Z |
| BTST.C Ws,bit4 | Bit Test Ws to C | 0.5/1 | 1 | C, Z | ||
| BTST.Z Ws,bit4 | Bit Test Ws to Z | 1 | 1 | Z | ||
| BTST.C Ws,Wb | Bit Test Ws<Wb> to C | 0.5/1 | 1 | C, Z | ||
| BTST.Z Ws,Wb | Bit Test Ws<Wb> to Z | 1 | 1 | Z | ||
| 19 | BTSTS | BTSTS.b f,bit3 | Bit Test then Set f | 1 | 1 | Z |
| BTSTS.C Ws,bit4 | Bit Test Ws to C then Set | 0.5/1 | 1 | C, Z | ||
| BTSTS.Z Ws,bit4 | Bit Test Ws to Z then Set | 1 | 1 | Z | ||
| 20 | CALL | CALL Label | Call subroutine (label > ~ 16MB) | 1 | 1 | None |
| Call subroutine (label < ~ 16MB) | 2 | 2 | None | |||
| CALL Wns | Call indirect subroutine at address [W11] | 1 | 2 | None | ||
| 21 | CLR | CLR f | f = 0x0000 0000 | 1 | 1 | None |
| CLR Wd | Wd = 0x0000 0000 | 1 | 1 | None | ||
| CLR A | Clear Accumulator | 0.5 | 1 | None | ||
| 21 | CLRWDT | CLRWDT | Clear Watchdog Timer | 0.5 | 1 | WDTO, Sleep |
| 22 | COM | COM f | f = f | 1 | 1 | N, Z |
| COM f,Wd | Wd = f | 1 | 1 | N, Z | ||
| COM Ws,Wd | Wd = Ws | 0.5/1 | 1 | N, Z | ||
| 23 | CP | CP f,Ws | Compare f with Ws | 1 | 1 | C, N, OV, Z |
| CP Ws,#lit13 | Compare Ws with lit13 (literal zeroextended) | 1 | 1 | C, N, OV, Z | ||
| CP Wb,#lit16 | Compare Wb with lit16 (literal zeroextended) | 1 | 1 | C, N, OV, Z | ||
| CP Wb, Ws | Compare Wb with Ws | 0.5/1 | 1 | C, N, OV, Z | ||
| 24 | CP0 | CP0 f | Compare f with 0x0000 0000 | 1 | 1 | C, N, OV, Z |
| CP0 Ws | Compare Ws with 0x0000 0000 (substitute CPLS Ws ,#0) | 1 | 1 | C, N, OV, Z | ||
| 25 | CPB | CPB f,Ws | Compare f with Ws, with borrow | 1 | 1 | C, N, OV, Z |
| CP Wb,#lit13 | Compare Wb with lit13, with borrow (literal zero-extended) | 1 | 1 | C, N, OV, Z | ||
| CP Wb,#lit16 | Compare Wb with lit16, with borrow (literal zero-extended) | 1 | 1 | C, N, OV, Z | ||
| CPB Wb,Ws | Compare Borrow Wb with Ws | 0.5/1 | 1 | C, N, OV, Z | ||
| CPSEQ | Not supported | N/A | ||||
| CPBEQ | Not supported | N/A | ||||
| CPSGT | Not supported | N/A | ||||
| CPBGT | Not supported | N/A | ||||
| CPSNE | Not supported | N/A | ||||
| 26 | CTXTSWP | CTXTSWP #lit3 | Swap to CPU register context defined by lit3 | 0.5 | 2 | None |
| CTXTSWP Wn | Swap to CPU register context defined in Wn[2:0] | 1 | 2 | None | ||
| 27 | DAW | Not supported | N/A | |||
| 28 | DEC | DEC f | f = f -1 | 1 | 1 | C, N, OV, Z |
| DEC f,Wd | W5 = f -1 | 1 | 1 | C, N, OV, Z | ||
| DEC Ws,Wd | Wd = Ws - 1 | 1 | 1 | C, N, OV, Z | ||
| 29 | DEC2 | DEC2 f | f = f -2 | 1 | 1 | C, N, OV, Z |
| DEC2 f,Wd | W5 = f -2 | 1 | 1 | C, N, OV, Z | ||
| DEC2 Ws,Wd | Wd = Ws - 2 | 1 | 1 | C, N, OV, Z | ||
| 30 | DISI | Not supported | N/A | |||
| 31 | DISICTL | DISICTL #lit3 {,Wd} | Disable interrupts at IPL <= lit3 Optionally save prior IPL threshold to Wd | 1 | 1 | None |
| DISICTL Wns {,Wd} | Disable interrupts at IPL <= Wns[2:0] Optionally save prior IPL threshold to Wd | 1 | 1 | None | ||
| 32 | DIVF | DIVF Wm/Wn | Interruptible Signed 16/16 or 32/16 Fractional Divide | 1 | 1 | C, N, OV, Z |
| 33 | DIVFL | DIVFL Wm/Wn | Interruptible Signed 32/32 Fractional Divide | 1 | 1 | C, N, OV, Z |
| 34 | DIVS | DIVS.w Wm/Wn | Interruptible Signed 16/16-bit Integer Divide | 1 | 1 | C, N, OV, Z |
| DIVS.l Wm/Wn | Interruptible Signed 32/16-bit Integer Divide | 1 | 1 | C, N, OV, Z | ||
| 35 | DIVSL | DIVSL Wm/Wn | Interruptible Signed 32/32 Integer Divide | 1 | 1 | C, N, OV, Z |
| 36 | DIVU | DIVU.w Wm/Wn | Interruptible Unsigned 16/16-bit Integer Divide | 1 | 1 | C, N, OV, Z |
| DIVU.l Wm/Wn | Interruptible Unsigned 32/16-bit Integer Divide | 1 | 1 | C, N, OV, Z | ||
| 37 | DIVUL | DIVUL Wm/Wn | Interruptible Unsigned 32/32 Integer Divide | 1 | 1 | C, N, OV, Z |
| 38 | DIV2 | Not supported | N/A | |||
| 39 | DTB | DTB Wn,Label | Decrement Wn, then branch if not zero | 1 | 1(2/3) | None |
| 40 | DO | Not supported | N/A | |||
| 41 | ED | ED Wxp * Wyp, A, AWB | Euclidean Distance | 1 | 2 | OA, SA, OB, SB |
| 42 | EDAC | EDAC Wxp * Wyp, A, AWB | Euclidean Distance Accumulate | 1 | 2 | OA, SA, OB, SB |
| 43 | EXCH | EXCH Wns,Wnd | Swap Wns with Wnd | 1 | 2 | None |
| 44 | FBCL | FBCL Ws,Wnd | Find Bit Change from Left (MSb) Side | 1 | 1 | C |
| 45 | FF1L | FF1L Ws,Wnd | Find First One from Left (MSb) Side | 1 | 1 | C |
| 46 | FF1R | FF1R Ws,Wnd | Find First One from Right (LSb) Side | 1 | 1 | C |
| 47 | FLIM | FLIM Wb, Ws | Force Data (Upper and Lower) Range Limit without Limit Excess Result | 1 | 2 | N, Z, OV |
| FLIM Wb, Ws, Wd | Force Data (Upper and Lower) Range Limit with Limit Excess Flag (Wd=-1) | 1 | 2 | N, Z, OV | ||
| FLIM.V Wb, Ws, Wd | Force Data (Upper and Lower) Range Limit with Limit Excess Result | 1 | 2 | N, Z, OV | ||
| 48 | GOTO | GOTO Label | Goto address (address < ~ 16MB) | 1 | 2 | None |
| GOTO Label | (label < ~ 16MB) | 2 | 2 | None | ||
| GOTO Wn | Go to indirect address at [W11] | 1 | 2 | None | ||
| 49 | INC | INC f | f = f + 1 | 1 | 1 | C, N, OV, Z |
| INC f,Wd | W5 = f + 1 | 1 | 1 | C, N, OV, Z | ||
| INC Ws,Wd | Wd = Ws + 1 | 1 | 1 | C, N, OV, Z | ||
| 50 | INC2 | INC2 f | f = f + 2 | 1 | 1 | C, N, OV, Z |
| INC2 f,Wd | W5 = f + 2 | 1 | 1 | C, N, OV, Z | ||
| INC2 Ws,Wd | Wd = Ws +2 | 1 | 1 | C, N, OV, Z | ||
| 51 | IOR | IOR f,Wn | f = f .IOR. Wn | 1 | 1 | N, Z |
| IOR f,Wn,Wn | Wn = f .IOR. Wn | 1 | 1 | N, Z | ||
| IOR #lit16,Wn | Wn = Wn .IOR. lit16 | 1 | 1 | N, Z | ||
| IOR Wb,Ws,Wd | Wd = Wb .IOR. Ws | 0.5/1 | 1 | N, Z | ||
| IOR Wb,#lit7,Wd | Wd = Wb .IOR. lit7 | 1 | 1 | N, Z | ||
| 52 | LAC | LAC Rso,#Slit6, A | Load Accumulator (16/32-bit), literal shift | 1 | 1 | OA, SA, OB, SB |
| LLAC | LLAC.l Rso,#Slit6, A | Load Lower (LSw) of Accumulator (32-bit), literal shift | 1 | 1 | OA, SA, OB, SB | |
| LAUC | LUAC.l Rso,#Slit6, A | Load Upper (LSb) of Accumulator (32-bit), literal shift | 1 | 1 | OA, SA, OB, SB | |
| 53 | LNK | LNK #lit16 | Link frame pointer | 1 | 1 | None |
| LNK #lit7 | Link frame pointer (literal < 128) | 0.5 | 1 | None | ||
| 54 | LSR | LSR f | f = Logical Right Shift f by 1 | 1 | 1 | C,N,Z |
| LSR f,Wd | Wd = Logical Right Shift f by 1 | 1 | 1 | C,N,Z | ||
| LSR Ws,Wd | Wd = Logical Right Shift Ws by 1 | 0.5/1 | 1 | C,N,Z | ||
| LSR Ws,Wb,Wd | Wnd = Logical Right Shift Ws by Wns | 0.5/1 | 1 | C,N,Z | ||
| LSR Ws,#lit5,Wd | Wnd = Logical Right Shift Ws by lit5 | 0.5/1 | 1 | N,Z | ||
| LSRM Ws,#lit5, Wnd | Wnd = Logical Right Shift Ws by lit5, then logically OR with next lsw | 1 | 2 | N,Z | ||
| LSRM Ws, Wb, Wnd | Wnd = Logical Right Shift Ws by Wb, then logically OR with next lsw | 1 | 2 | N,Z | ||
| 55 | MAC | MAC Wxp * Wyp, A, AWB | Multiply and Accumulate | 1 | 1 | OA, SA, OB, SB |
| 56 | MAX | MAX Wb, Ws | Force Data Maximum Range Limit | 1 | 1 | OA, SA, OB, SB |
| MAX A | Force Data Maximum Range Limit | 0.5 | 1 | N, Z, OV | ||
| MAX.V A, Rdo | Force Data Maximum Range Limit with Result | 1 | 2 | N, Z, OV | ||
| 57 | MIN | MIN Wb, Ws | Force Data Minimum Range Limit | 1 | 1 | N, Z, OV |
| MIN A | Force Data Minimum Range Limit | 0.5 | 1 | N, Z, OV | ||
| MIN.V A, Rdo | Force Data Minimum Range Limit with Result | 1 | 2 | N, Z, OV | ||
| 58 | MOV | MOV Rso,Rdo | Move Ws to Wd | 0.5/1 | 1 | None |
| MOV.l #lit32,Wnd | Move 32-bit unsigned literal to Wnd | 2 | 2 | None | ||
| MOV.sl #lit24,Wnd | Move 24-bit unsigned literal to Wnd; 0 extend to 32-bits | 1 | 1 | None | ||
| MOV.w #lit16,Wnd | Move 16-bit unsigned literal to Wnd; 0 extend to 32-bits | 1 | 1 | None | ||
| MOV.bz #lit8,Wnd | Move 8-bit unsigned literal to Wnd; 0 extend to 32-bits | 1 | 1 | None | ||
| MOV.l [W15-#lit7], Wnd [W14+#slit7], Wnd | Move from system stack with literal offset to Wnd using SP or FP | 0.5 | 1 | None | ||
| MOV.l Wns, [W15-#lit7] Wns, [W14+#slit7] | Move from Wns to system stack with literal off-set using SP or FP | 0.5 | 1 | None | ||
| MOV.l f,Wnd | Move f to Wnd (Word or Long Word)(f < ~1MB) | 1 | 1 | None | ||
| MOV.w f,Wnd | Move f to Wnd (Word or Long Word)(f > ~1MB) | 2 | 2 | None | ||
| MOV.b f,Wnd | Move f to Wnd (Byte) | 1 | 1 | None | ||
| MOV.l Wns,f | Move Wns to f (Word or Long Word)(f < ~1MB) | 1 | 1 | None | ||
| MOV.w Wns,f | Move Wns to f (Word or Long Word)(f > ~1MB) | 2 | 2 | None | ||
| MOV.b Wns,f | Move Wns to f (Byte) | 1 | 1 | None | ||
| MOV [Wns+#Slit12],Wnd | Move [Wns+Slit12] to Wnd | 1 | 1 | None | ||
| MOV Wns,[Wnd+#Slit12] | Move Wns to [Wnd+Slit12] | 1 | 1 | None | ||
| MOVIF.l CC, Wb, Wns, Wd | If SR.Z=1 Move W1 to [W15++] Else Move W2 to [W15++] | 1 | 1 | None | ||
| MOVIF.w CC, Wb, Wns, Wd | If SR.Z=1 Move W1 to [W15++] Else Move W2 to [W15++] | 1 | 1 | None | ||
| MOVIF.bz CC, Wb, Wns, Wd | If SR.Z=1 Move W1 to [W15++] Else Move W2 to [W15++] | 1 | 1 | None | ||
| MOVIF.b CC, Wb, Wns, Wd | If SR.Z=1 Move W1 to [W15++] Else Move W2 to [W15++] | 1 | 1 | None | ||
| MOVR.l | Move Ws to Wd with destination Bit Reversed | 1 | 1 | None | ||
| MOVR.w | Move Ws to Wd with destination Bit Reversed | 1 | 1 | None | ||
| MOVS.l #slit16, Wd | Move signed extended 16-bit literal to Wd | 1 | 1 | None | ||
| MOVS.w #slit16, Wd | Move 16-bit literal to Wd; sign extend to 32-bits if register direct mode. | 1 | 1 | None | ||
| MOVS.b #slit8, Wnd | Move 8-bit literal to Wd; no extension. | 1 | 1 | None | ||
| 59 | MOVPAG | Not supported | N/A | |||
| 60 | MOVSAC | Not supported | N/A | |||
| 61 | MPY | MPY Wxp * Wyp, A, AWB | Multiply Wm by Wn to Accumulator | 1 | 1 | OA, SA, OB, SB |
| 62 | MPYN | MPYN Wxp * Wyp, A, AWB | (negative)(Multiply Wm by Wn) to Accumulator | 1 | 1 | OA, SA, OB, SB |
| 63 | MSC | MSC Wxp * Wyp, A, AWB | Multiply and Subtract from Accumulator | 1 | 1 | OA, SA, OB, SB |
| 65 | MUL | MUL f, Wn | W2 = f * Wn | 1 | 1 | None |
| MULISS Wb,Ws,A | Integer: Acc(A or B) = signed(Wb) * signed(Ws) | 1 | 1 | None | ||
| MULFSS Wb,Ws,A | Fractional: Acc(A or B) = signed(Wb) * signed(Ws) | 1 | 1 | None | ||
| MULISU Wb,Ws,A | Integer: Acc(A or B) = signed(Wb) * unsigned(Ws) | 1 | 1 | None | ||
| MULFSU Wb,Ws,A | Fractional: Acc(A or B) = signed(Wb) * unsigned(Ws) | 1 | 1 | None | ||
| MULIUS Wb,Ws,A | Integer: Acc(A or B) = unsigned(Wb) * signed(Ws) | 1 | 1 | None | ||
| MULFUS Wb,Ws,A | Fractional: Acc(A or B) = unsigned(Wb) * signed(Ws) | 1 | 1 | None | ||
| MULIUU Wb,Ws,A | Integer: Acc(A or B) = unsigned(Wb) * unsigned(Ws) | 1 | 1 | None | ||
| MULFUU Wb,Ws,A | Fractional: Acc(A or B) = unsigned(Wb) * unsigned(Ws) | 1 | 1 | None | ||
| MULISS Wb,#slit8,A | Integer: Acc(A or B) = signed(Wb) * signed(slit8) | 1 | 1 | None | ||
| MULFSS Wb,#slit8,A | Integer: Acc(A or B) = signed(Wb) * signed(slit8) | 1 | 1 | None | ||
| MULISU Wb,#lit8,A | Integer: Acc(A or B) = signed(Wb) * unsigned(lit8) | 1 | 1 | None | ||
| MULFSU Wb,#lit8,A | Integer: Acc(A or B) = signed(Wb) * unsigned(lit8) | 1 | 1 | None | ||
| MULIUS Wb,#slit8,A | Integer: Acc(A or B) = signed(Wb) * signed(slit8) | 1 | 1 | None | ||
| MULFUS Wb,#slit8,A | Integer: Acc(A or B) = signed(Wb) * signed(slit8) | 1 | 1 | None | ||
| MULIUU Wb,#lit8,A | Integer: Acc(A or B) = signed(Wb) * unsigned(lit8) | 1 | 1 | None | ||
| MULFUU Wb,#lit8,A | Integer: Acc(A or B) = signed(Wb) * unsigned(lit8) | 1 | 1 | None | ||
| MULSS Wb,Ws,Wnd | {Wd}=signed(Wb) * signed(Ws) | 0.5/1 | 1 | None | ||
| MULSU Wb,Ws,Wnd | {Wd}=signed(Wb) * unsigned(Ws) | 0.5/1 | 1 | None | ||
| MULUS Wb,Ws,Wnd | {Wd}=unsigned(Wb) * signed(Ws) | 0.5/1 | 1 | None | ||
| MULUU Wb,Ws,Wnd | {Wd}=unsigned(Wb) * unsigned(Ws) | 0.5/1 | 1 | None | ||
| MULSU Wb,#lit8,Wnd | {Wd}=signed(Wb) * unsigned(lit8) | 1 | 1 | None | ||
| MULUU Wb,#lit8,Wnd | {Wd}=unsigned(Wb) * unsigned(lit8) | 1 | 1 | None | ||
| MULSS Wb,#slit8,Wnd | {Wd}=signed(Wb) * signed(slit8) | 1 | 1 | None | ||
| MULUS Wb,#slit8,Wnd | {Wd}=unsigned(Wb) * signed(slit8) | 1 | 1 | None | ||
| 66 | NEG | NEG A | Negate Accumulator | 1 | 1 | OA, SA, OB, SB |
| NEG f | f = f +1 | 1 | 1 | OA, SA, OB, SB | ||
| NEG f,Wd | Wd = f + 1 | 1 | 1 | OA, SA, OB, SB | ||
| NEG Ws,Wd | Wd = Ws + 1 | 1 | 1 | OA, SA, OB, SB | ||
| 67 | NEOP | NEOP | None executable NOP (16-bit instruction pad) | 0.5 | 0 | None |
| 68 | NOP | NOP | No Operation | 1 | 1 | None |
| NOPR | No Operation | 1 | 1 | None | ||
| 69 | NORM | NORM A, Rdo | Normalize Accumulator | 1 | 1 | N,OV,Z |
| 70 | POP | POP f | Pop f from top of stack (TOS) | 1 | 1 | None |
| POP {[--Ws],} Wnd | Pop Wnd Register from system stack. | 0.5 | 1 | None | ||
| POP Fd | Pop Fd Register from system stack. | 0.5 | 1 | None | ||
| 71 | PUSH | PUSH f | Push f to top of stack (TOS) | 1 | 1 | None |
| PUSH Wns, {[Wd++]} | Push Wns Register to system stack | 0.5 | 1 | None | ||
| PUSH Fs | Push Fs Register to system stack | 0.5 | 1 | None | ||
| 72 | PWRSAV | PWRSAV mode | Go into sleep mode | 0.5 | 2 | WDTO, Sleep |
| RCALL | RCALL Label | Relative Call | 1 | 1 | None | |
| RCALL Wns | Computed Call | 1 | 2 | None | ||
| 73 | REPEAT | REPEAT #lit15 | Repeat Next Instruction lit15+1 times | 1 | 1 | RA (if lit15 > 0) |
| REPEAT #lit5 | Repeat Next Instruction lit5+1 times | 0.5 | 1 | RA (if lit5 > 0) | ||
| REPEAT Wn | Repeat Next Instruction (Wn)+1 times | 1 | 1 | RA (if Wn > 0) | ||
| 74 | RESET | RESET | Software Device Reset | 1 | 1 | None |
| 75 | RETFIE | RETFIE | Return from interrupt enable | 1 | 4 | None |
| 76 | RETLW lit16,Wn | RETLW #lit16,Wn | Return from Subroutine with literal in Wn | 1 | 3 | None |
| 77 | RETURN | RETURN | Return from Subroutine | 0.5 | 3 | None |
| 78 | RLC | RLC f | f = Rotate Left through Carry f | 1 | 1 | C, N, Z |
| RLC f,Wd | Wd = Rotate Left through Carry f | 1 | 1 | C, N, Z | ||
| RLC Ws,Wd | Wd = Rotate Left through Carry Ws | 0.5/1 | 1 | C, N, Z | ||
| 79 | RLNC | RLNC f | f = Rotate Left (No Carry) f | 1 | 1 | N, Z |
| RLNC f,Wd | Wd = Rotate Left (No Carry) f | 1 | 1 | N, Z | ||
| RLNC Ws,Wd | Wd = Rotate Left (No Carry) Ws | 0.5/1 | 1 | N, Z | ||
| 80 | RRC | RRC f | f = Rotate Right through Carry f | 1 | 1 | C, N, Z |
| RRC f,Wd | Wd = Rotate Right through Carry f | 1 | 1 | C, N, Z | ||
| RRC Ws,Wd | Wd = Rotate Right through Carry Ws | 0.5/1 | 1 | C, N, Z | ||
| 81 | RRNC | RRNC f | f = Rotate Right (No Carry) f | 1 | 1 | N, Z |
| RRNC f,Wd | Wd = Rotate Right (No Carry) f | 1 | 1 | N, Z | ||
| RRNC Ws,Wd | Wd = Rotate Right (No Carry) Ws | 0.5/1 | 1 | N, Z | ||
| 82 | SAC | SAC A,#Slit6,Rdo | Store Accumulator (16/32-bit) | 1 | 1 | None |
| SACR A,#Slit6,Rdo | Store Rounded Accumulator (16/32-bit), literal shift | 1 | 1 | None | ||
| SACRW A,Ws,Rdo | Store Rounded Accumulator (16/32-bit), Wb shift | 1 | 1 | None | ||
| 83 | SE | SE Rso,Wnd | Wd = sign-extended Ws | 0.5/1 | 1 | C, N, Z |
| 84 | SETM | SETM f | f = 0xFFFF FFFF | 1 | 1 | None |
| SETM Wd | Wd = 0xFFFF FFFF | 1 | 1 | None | ||
| 85 | SFTAC | SFTAC A,Wn | Arithmetic Shift by (Wn) Accumulator | 1 | 1 | OA, SA, OB, SB |
| SFTAC A,#Slit7 | Arithmetic Shift by Slit7 Accumulator | 1 | 1 | OA, SA, OB, SB | ||
| 86 | SL | SL f | f = Left Shift f by 1 | 1 | 1 | C, N, Z |
| SL f,Wd | Wd = Left Shift f by 1 | 1 | 1 | C, N, Z | ||
| SL Ws,Wd | Wd = Left Shift Ws by 1 | 0.5/1 | 1 | C, N, Z | ||
| SL Ws,Wb,Wnd | Wnd = Left Shift Wb by Wns | 0.5/1 | 1 | C, N, Z | ||
| SL Ws,#lit5,Wnd | Wnd = Left Shift Ws by lit5 | 0.5/1 | 1 | C, N, Z | ||
| SLM | SLM Ws, #lit5, Wnd | Wnd = Left Shift Wb by lit5, then logically OR with next msw | 1 | 2 | Z | |
| SLM Ws, Wb, Wnd | Wnd = Left Shift Wb by Wb, then logically OR with next msw | 1 | 2 | Z | ||
| 87 | SLAC | SLAC.l A,#Slit6,Rdo | Store Lower (lsw of) Accumulator (32-bit), literal shift | 1 | 1 | None |
| 88 | SUAC | SUAC.l A,#Slit6,Rdo | Store sign extended Upper (MSB) Accumulator (32- bit), literal shift | 1 | 1 | None |
| 89 | SUB | SUB A | Subtract Accumulators | 0.5 | 1 | OA, SA, OB, SB |
| SUB Rso,#Slit6, A | 16-bit Signed Subtract from Accumulator | 1 | 1 | OA, SA, OB, SB | ||
| SUB f,Wn | f = f - Wn | 1 | 1 | C, N, OV, Z | ||
| SUB f,Wn,Wn | Wn = f - Wn | 1 | 1 | C, N, OV, Z | ||
| SUB.l #lit5,Wn | Wn = Wn - lit5 | 0.5 | 1 | C, N, OV, Z | ||
| SUB #lit16,Wn | Wn = Wn - lit16 | 1 | 1 | C, N, OV, Z | ||
| SUB Wb,Ws,Wd | Wd = Wb - Ws | 0.5/1 | 1 | C, N, OV, Z | ||
| SUB Ws,#lit7,Wd | Wd = Ws - lit7 (literal zero-extended) | 1 | 1 | C, N, OV, Z | ||
| 90 | SUBB | SUBB f,Wn | f = f - Wn - (C) | 1 | 1 | C, N, OV, Z |
| SUBB f,Wn,Wn | Wn = f - Wn - (C) | 1 | 1 | C, N, OV, Z | ||
| SUBB #lit16,Wn | Wn = Wn - lit16 - (C) | 1 | 1 | C, N, OV, Z | ||
| SUBB Wb,Ws,Wd | Wd = Wb - Ws - (C) | 0.5/1 | 1 | C, N, OV, Z | ||
| SUBB Ws,#lit7,Wd | Wd = Ws - lit7 - (literal zero-extended) | 1 | 1 | C, N, OV, Z | ||
| 91 | SUBR | SUBR f,Wn | f = Wn - f | 1 | 1 | C, N, OV, Z |
| SUBR f,Wn,Wn | Wn = Wn - f | 1 | 1 | C, N, OV, Z | ||
| SUBR Wb,Ws,Wd | Wd = Ws - Wb | 0.5/1 | 1 | C, N, OV, Z | ||
| SUBR Ws,#lit7,Wd | Wd = lit7 - Ws (literal zero-extended) | 0.5/1 | 1 | C, N, OV, Z | ||
| 92 | SUBBR | SUBBR f,Wn | f = Wn - f - (C) | 1 | 1 | C, N, OV, Z |
| SUBBR f,Wn,Wn | Wn = Wn -f - (C) | 1 | 1 | C, N, OV, Z | ||
| SUBBR Wb,Ws,Wd | Wd = Ws - Wb - (C) | 0.5/1 | 1 | C, N, OV, Z | ||
| SUBBR Ws,#lit7,Wd | Wd = lit7 - Ws - (C) (literal zero-extended) | 1 | 1 | C, N, OV, Z | ||
| 93 | SWAP | SWAP Wn | Wn = Word or byte swap Wn | 1 | 1 | None |
| 94 | SQR | SQR Wxp, A, AWB | Square to Accumulator | 1 | 1 | OA, SA, OB, SB |
| 95 | SQRAC | SQRAC Wxp, A, AWB | Square and Accumulate | 1 | 1 | OA, SA, OB, SB |
| 96 | SQRN | SQRN Wxp, A, AWB | Negated Square to Accumulator | 1 | 1 | OA, SA, OB, SB |
| 97 | SQRSC | SQRSC Wxp, A, AWB | Square and Subtract from Accumulator | 1 | 1 | OA, SA, OB, SB |
| 98 | TBLRDH | Not supported | N/A | |||
| 99 | TBLRDL | Not supported | N/A | |||
| 100 | TBLWTH | Not supported | N/A | |||
| 101 | TBLWTL | Not supported | N/A | |||
| 102 | TST | TST f | Test f | 1 | 1 | N, Z |
| TST f,Wnd | Test f and move f to Wnd | 1 | 1 | N, Z | ||
| 103 | ULNK | ULNK | Unlink frame pointer | 1 | 1 | None |
| 104 | XOR | XOR f,Wn | f = f .XOR. Wn | 1 | 1 | N, Z |
| XOR f,Wn,Wn | Wn = f .XOR. Wn | 1 | 1 | N, Z | ||
| XOR lit16,Wn | Wn = Wn .XOR. lit16 | 1 | 1 | N, Z | ||
| XOR Wb,Ws,Wd | Wd = Wb .XOR. Ws | 0.5/1 | 1 | N, Z | ||
| XOR Wb,lit7,Wd | Wd = Wb .XOR. Lit7 (literal zero-extended) | 1 | 1 | N, Z | ||
| 105 | ZE | ZE Rso,Wnd | Wd = Zero-extend Ws | 0.5/1 | 1 | C, N, Z |
|
Note:
| ||||||