3.3.4.38 USB_HOST_AUDIO_V1_StreamingInterfaceTerminalLinkGet Function

C

uint8_t USB_HOST_AUDIO_V1_StreamingInterfaceTerminalLinkGet(
    USB_HOST_AUDIO_V1_OBJ audioObj, 
    USB_HOST_AUDIO_V1_STREAMING_INTERFACE_OBJ streamingInterfaceObj, 
    USB_HOST_AUDIO_V1_STREAMING_INTERFACE_SETTING_OBJ interfaceSettingObj
);

Summary

This function returns the terminal link of the specified streaming interface setting.

Precondition

The Audio v1.0 Device should have been attached.

Parameters

Parameters Description
audioObj Audio Device object
streamingInterfaceObj Audio streaming interface object
interfaceSettingObj Audio streaming interface setting object

Returns

The terminal link of the audio streaming interface setting.

Remarks

None.