12.5.4 Use Preset Passkey Parameter
The use preset passkey parameter enables the IS187x device to use a pre-programmed passkey value for the passkey entry pairing method.
- Enable – The user provides a six-digit passkey value (represented as ASCII characters) in the Passkey Value Parameter. For more details, refer to Passkey Value Parameter.
- Disable – The passkey entry is the pairing method used during the pairing process, and the IS187x device generates a random six-digit value.
The IS187x device makes the external host MCU aware of the passkey value by sending the six-digit value using the appropriate command from the command set protocol. For more details, refer to the Bluetooth Core Specification (4.2), volume 3, part H.
| Parameter | Value | Parameter Description | Length |
|---|---|---|---|
| Bit 0 | System option 2 Bit[0] |
| 1 bit |
Operational Mode
This system option 2 parameter can affect the behavior in Manual or Auto Operation mode. The programming of the parameter affects the behavior.