12 Serial Quad Interface (SQI)
DDR
SQI Dual and Quad mode Double Data Rate (DDR) write modes are inoperative.
Workaround
None.
Affected Silicon Revisions
| A1 | A2 | ||||
|---|---|---|---|---|---|
| X | - |
XIP
Byte and half-word transfers are not supported in XIP mode.
Workaround
When using XIP mode, transfer access should be limited to the word size.
Affected Silicon Revisions
| A1 | A2 | ||||
|---|---|---|---|---|---|
| X | X |
DMA
When using a DMA descriptor with the Status Polling Option bit set, the PKTCOMPIF interrupt flag will be set before the status check has completed.
Workaround
- Disable the interrupts for the descriptor that uses status check.
- Add a new descriptor (preferably read) to the list right after the one with the status check bit set.
- Set the interrupt enable on this descriptor CBD_INT_EN and PKT_INT_EN.
- The execution of this descriptor will only happen after the previous one is complete (including its corresponding status check).
- Use the PKTCOMPIF, which will be set after the whole operation has completed.
Note: Ensure to manually clear
PKTCOMPIF when starting a DMA operation.
Affected Silicon Revisions
| A1 | A2 | ||||
|---|---|---|---|---|---|
| X | X |