6.23.53 wcstoll Function
Convert wide string to a long long integer value.
Include
<wchar.h>
Prototype
long long int wcstoll(const wchar_t * restrict nptr, wchar_t ** restrict
endptr, int base);
Arguments
nptr- the wide string to attempt to convert
endptr- pointer to store the address of the remainder of the wide string that was not converted
base- the radix in which the value of the wide string should be interpreted
Return Value
The converted value, or 0 if the conversion could not be performed. If the correct value of
the conversion is outside the range of representable values, LLONG_MIN or
LLONG_MAX is returned based on the sign of the correct value.
Remarks
The wcstoll function attempts to convert a portion of the wide string
pointed to by nptr to a long long intvalue.
The initial sequence consists of any white-space wide characters.
The subject sequence represents the integer constant to convert and whose radix is
given by base.
If the value of base is zero, the expected form of the subject
sequence is that of an integer constant whose radix is determined by the sequence
itself. For example, a leading 0x implies a hexadecimal constant; a
leading 0 implies an octal constant. The sequence may be preceded
by a plus or minus sign, but not including an integer suffix.
If the value of base is between 2 and 36 (inclusive), the expected
form of the subject sequence is a sequence of letters (a (or
A) through z (or Z) ascribed
the values 10 through 35) and digits representing an integer with the radix
specified by base. Only letters and digits whose ascribed values
are less than that of base are permitted. The sequence may be
preceded by a plus or minus sign, but not including an integer suffix. If the value
of base is 16, the wide characters 0x or
0X may prefix the sequence of letters and digits, following the
sign wide character if present.
Conversion stops once an unrecognized wide character is encountered, thus the subject
sequence is defined as the longest subsequence of the input wide string after the
initial sequence and that is of the expected form. A pointer to the position of the
first unrecognizable wide character in the wide string is stored in the object
pointed to by endptr, provided that endptr is not
a null pointer.
The final sequence consists of wide characters in the wide string that were
unrecognized in the subject sequence and which will include the terminating null
wide character of the wide string. This sequence of the wide string will be
accessible via the address stored to endptr, provided
endptr is not a null pointer.
The value of the macro ERANGE is stored in errno if
the correct value of the conversion is outside the range of representable
values.
Example
#include <wchar.h>
int main ()
{
wchar_t ws[] = L"2001 60c0c0 -1101110100110100100000 7000 07000";
wchar_t * pEnd;
long long int lli1, lli2, lli3, lli4, lli5;
lli1 = wcstoll(ws, &pEnd, 10);
lli2 = wcstoll(pEnd, &pEnd, 16);
lli3 = wcstoll(pEnd, &pEnd, 2);
lli4 = wcstoll(pEnd, &pEnd, 16);
lli5 = wcstoll(pEnd, NULL, 0);
wprintf(L"The converted string values in decimal are: %lld, %lld, %lld, %lld, and %lld.\n", lli1, lli2, lli3, lli4, lli5);
}
Example Output
The converted string values in decimal are: 2001, 6340800, -3624224, 28672, and 3584.