6.23.16 mbrlen Function
Determines the length of a multibyte character.
Include
<wchar.h>
Prototype
size_t mbrlen(const char * restrict s, size_t n, mbstate_t * restrict
ps);
Arguments
s- a pointer to the multibyte character to check
n- the maximum number of bytes to check
ps- a pointer to a
mbstate_tobject that holds the current conversion state
Return Value
The function returns the length of a multibyte sequence between 0 and n
inclusive, representing the length; or the value -1 or -2, as per the
mbrtowc() function. nonzero if ps is a null pointer or if
the pointed-to object describes an initial conversion state; otherwise, it returns zero.
Remarks
An object of type mbstate_t is used to describe the current conversion state
from a particular multibyte character sequence to a wide character sequence (or the reverse
conversion) based on the current locale. For both conversions, the initial conversion state
corresponds to the beginning of a new multibyte character in the initial shift state. A
zero-valued mbstate_t always represents an initial conversion state.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <wchar.h>
#include <stdlib.h>
#include <string.h>
int main(void)
{
char * string = "The final frontier";
mbstate_t state = {0};
wchar_t wc;
mbrtowc(&wc, string, MB_CUR_MAX, &state);
if(mbsinit(&state)) // check initial conversion state
wprintf(L"In initial conversion state\n");
else
memset(&state, 0, sizeof(state)); // set initial conversion state
}
Example Output
In initial conversion state