6.23.9 fputwc Function
Writes a wide character to a stream.
Include
<wchar.h>
Prototype
wint_t fputwc(wchar_t c, FILE * stream);
Arguments
c- the wide character to write
stream- the stream to write to
Return Value
The function returns a copy of the wide character written. If a write or encoding error
occurs, WEOF is returned.
Remarks
The function writes the wide character, c, to the output stream pointed to
by stream and at the position indicated by the file position indicator for the stream (if
defined), advancing the indicator appropriately. If positioning within the file is not
supported or if the stream was opened with append mode, the character is appended to the
output stream.
The error indicator for the stream will be set on a write error. If an encoding error
occurs, errno is set to the value of the EILSEQ macro.
Example
#include <wchar.h>
#include <stdio.h>
int main(void)
{
FILE * myfile;
wint_t wc;
if ((myfile = fopen("afile", "w")) == NULL)
wprintf(L"Cannot open afile\n");
else
{
for(wc = L'0'; iswdigit(wc); wc++)
fputwc(wc, myfile);
fputwc(L'\n', myfile);
fclose(myfile);
}
}
Example Output
Content of afile.
0123456789