6.23.19 mbsrtowcs Function
Convert a multibyte character sequence to a wide character string.
Include
<wchar.h>
Prototype
size_t mbsrtowcs(wchar_t * restrict dst, const char ** restrict src,
size_t len, mbstate_t * restrict ps);
Arguments
dst- a pointer to the object to hold the converted wide character
src- the mulitbyte character sequence to convert
len- the maximum number of bytes to convert
ps- a pointer to a
mbstate_tobject that holds the current conversion state
Return Value
The function returns the number of multibyte characters successfully converted, not including
the terminating null character (if any). If src is not a valid multibyte
character sequence, (size_t)(-1) is returned.
Remarks
The function converts a sequence of multibyte characters indirectly pointed to by
src and that begins in the conversion state described by the object pointed
to by ps into a sequence of corresponding wide characters, storing the
converted characters (including a terminating null character) into the array pointed to by
dst, provided dst is not a null pointer, Conversion stops
when a terminating null wide character is encountered, when an invalid multibyte character
sequence is encountered, or when len wide characters have been stored. Each
conversion takes place as if by a call to the mbrtowc() function; however, by
having the argument to specify the current conversion state, this function is restartable.
An encoding error occurs if src is not a valid multibyte character sequence,
and the function stores the value of the macro EILSEQ in
errno and the conversion state is unspecified.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <locale.h>
#include <wchar.h>
#include <string.h>
void printWide(const char* mbstr)
{
mbstate_t state;
size_t len;
wchar_t wstr[40];
memset(&state, 0, sizeof state);
len = mbsrtowcs(&wstr[0], &mbstr, 40, &state);
wprintf(L"Converted wide string \"%ls\" has length %u\n", wstr, len);
}
int main(void)
{
setlocale(LC_CTYPE, "");
printWide("It is 75°F");
}
Example Output
Converted wide string "It is 75°F" has length 10