6.23.11 fwide Function
Sets and determines the width orientation of a stream.
Include
<wchar.h>
Prototype
int fwide(FILE * stream, int mode);
Arguments
stream- the stream to write to
mode- the stream orientation to set
Return Value
The function returns a positive value if, after the call, the stream has wide orientation, a negative value if the stream has byte orientation, or zero if the stream has no orientation.
Remarks
For positive values of mode, the function attempts to make the stream wide
oriented; for negative values, it attempts to make the stream byte oriented. For a
mode of zero, the orientation of the stream is not altered. Once a stream
has been oriented, subsequent calls to fwide() do not change that stream's
orientation.
Example
#include <wchar.h>
#include <stdio.h>
void prStrOrient(int orientation)
{
if (orientation > 0)
puts("The stream is wide oriented");
else if (orientation < 0)
puts("The stream is byte oriented");
else
puts("The stream is not oriented");
}
int main(void)
{
FILE * myfile;
int ret;
if ((myfile = fopen("afile", "w")) == NULL)
wprintf(L"Cannot open afile\n");
else {
ret = fwide(myfile, 0);
prStrOrient(ret);
ret = fwide(myfile, 1); // set wide orientation
prStrOrient(ret);
ret = fwide(myfile, -1); // no further changes made
prStrOrient(ret);
fclose (myfile);
}
}
Example Output
Content of afile.
The stream is not oriented
The stream is wide oriented
The stream is wide oriented