6.23.36 wcscpy Function
Copy a wide string to an array.
Attention: This function is implemented
only by MPLAB XC32 C compilers.
Include
<wchar.h>
Prototype
wchar_t * wcscpy( wchar_t * restrict s1, const wchar_t * restrict
s2);
Arguments
s1- the array to hold the copied wide string
s2- the wide string to copy
Return Value
A copy of s1.
Remarks
The function copies the wide string pointed to by s2 into the array
s1. The null wide character is copied.
Example
#include <wchar.h>
int main(void)
{
wchar_t ws[40];
wcscpy(ws, L"a literal wide string");
wprintf(L"the wide string referenced by ws is \"%ls\"\n", ws);
}
Example Output
the wide string referenced by ws is "a literal wide string"